大家好,我最近在做一个210kHz信号调理电路,原来板子上单端转差分使用的芯片是ADA4851-4,查看手册比较性能参数,发现ADA4807-4较ADA4851-4更好,这边想问下,能否用ADA4807-4替换原来的芯片,会不会有问题?
大家好,我最近在做一个210kHz信号调理电路,原来板子上单端转差分使用的芯片是ADA4851-4,查看手册比较性能参数,发现ADA4807-4较ADA4851-4更好,这边想问下,能否用ADA4807-4替换原来的芯片,会不会有问题?
Saludos. En este momento estoy trabajando con el amplificador ADA4807-4 (www.analog.com/.../ada4807-4.html), y necesito realizar análisis de integridad de la señal (SI), pero no puedo encontrar el modelo IBIS de este amplificador. ¿Alguien…
regards. At the moment I am working with the ADA4807-4 amplifier ( www.analog.com/.../ada4807-4.html ), and I need to performing Signal Integrity (SI) analyses, but I can not find the IBIS model of this amplifier. Can someone help me?
示波器上对信号做FFT分析,发现噪声稳定而且幅度不小,主要就是21Mhz及其2,3次谐波。
芯片的4运放,均设计的是同相放大2倍电路,输入信号由信号发生器给出的1.3Mhz,峰峰值1V,无直流偏置的的正弦波。
一个一个运放测试,输出结果都一样。不明白噪声源从何而来,而且这么固定。
Hi Hooman,
I change RF to 1.5K ohm (and other R along with RF) and clear path issue between source generator & non-inverting input. The oscillation issue of ADA4807-1 had been solved. I really appreciate your support.
Best Regards
Klex Lin
We are using the amplifier ADA4807-2 as an integrator. The ADA4807 is powerd from 6V. As an integrator the output is saturated to the rails. In our circuit it seems that the current consumption without any load increases with a few milliammperes when…
Dear Analog Devices
I am having challenge in understanding the datasheet on the ADA4807 (alternative AD8027), in respect of the output swing.
My challenge is that I have an input from a potmeter, providing a voltage input to a “buffer…
我选择ADA4807-1和ADA4807-4实现了数个滤波器电路和同向放大电路,但是我发现在每一个电路的输出都存在直流偏置,换成其他芯片(比如AD4096)这个偏置就会消失。请各位大牛帮我分析一下这个问题,感谢!
I created a lt spice model of my circuit which consists of an op amp in a unity gain voltage follower configuration which feeds a SAR ADC. I also included the flywheel circuit in front of the adc. There are two models, each one having a different op amp…