• (ADV7390/1)Does ADV7390/1 supports ED-SDR 8bits 54MHz?

    Hi!

    I have some questions about ADV739*.

    (1)=========================================================

    I want to input BT.656 ED(525p)-SDR 54MHz 8bit(not 16bit) to ADV739*.

    Does ADV7390/1 support that Video-format?

    Or must I use ADV7392/3?

    At the…

  • AD4110-1 Communication issue using development board EVAL-AD4110-1

    Hello all,

    I am facing issue in communicating with AD4110-1 via SPI pins in J2 connector on evaluation board using an external microcontroller. I am trying to read ID register as that register will be a static register hence it will be easy to know if…

  • What the difference between the ADA4940-1 and the ADA4941-1?

    What is the difference between the ADA4940-1 and the ADA4941-1? They are both ADC drivers, but what distinguishes the two parts from each other?

  • LTC2955-1 auto-turn-on disabled with 1 second VIN removal

    I have a circuit which allows for auto-turn-on with battery application. (SET = VIN, ON = VIN, PB floating, KILL_N = high.)

    It appears that I'm running into a problem with the datasheet statement "after the EN output goes low, the LTC2955-1 starts the…

  • LTM8055-1 compensation and capacitors

    Hi,

    as others here, I wanted to test the LTM8055-1 as a replacement for the used LTM8055. Just to have more options when there is a supply shortage of the LTM8055 at our suppliers.

    I created a 4 layer little board with the LTM8055-1 and all capacitors…

  • 看图说话,如何评价1+1>2

    近日,ADI正式完成对凌力尔特公司的并购。此次并购使ADI集双方的产品方案、客户群以及业内一流的工程设计、制造、销售、支持运营于一体,成为全球最具规模的领先模拟技术公司。实现1+1>2!

    ADI公司总裁兼首席执行官Vincent Roche表示:“ADI将与凌力尔特共同缔造一个模拟行业重量级企业。我们共同携手为客户解决在连接现实与数字领域所面临的更多巨大且复杂的挑战。未来,新ADI将为我们的客户、员工和股东在未来很多年内创造巨大的价值。”

    新ADI将有卓越的工程设计和高度互补的产品组合,一张图告诉你如何打造无与伦比的创新及增长驱动力…

  • LTC5588-1 LO Feedthrough Distribution at 6GHz

    Hi,

    Please if you can, provide data for the LTC5588-1 LO feedthrough distribution. Similar to graph 55881 G41.

    Thank you

  • RE: ADE9000 compliant with IEC 61010-1

    Hi John, The ADE9000 has no isolation so it does not meet 61010-1. Isolation would be needed like the an ADUM241E or the ADuM4150. Use the ade9000 eval board for reference.

    Dave

  • LTC4368-1 Bi-direction Current and Voltage Protection Issue

    To Analog Technical Support,

    Que1 -> We are using LTC4368-1 IC for Bi-directional voltage and current protection voltage ranging from

    UV=15V , OV=36V and Current -> -12.5A to +12.5A.

    Que-2-> UV=3V , OV=5V and Current -> -500mA to +500mA.…

  • 18 cells BMS with (LTC6813-1) and active balancer LTC3300-1 x3

    Dear Friends,

    We are planning to make 18 cells BMS with bidirectional active balancer. In order to that we are considering LTC6813-1 as 18 cell battery stack monitoring and LTC3300-1 x3 for link with active balancer. I have a few questions to clarify.