• .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • RE: Can't get data ADC data to be in [-1, 1) range on EZ-KIT SC589

    Hello,

    Hope you are discussing about this query via the below thread. Please continue the discussion there.

    ez.analog.com/.../can-t-cannot-transmit-adc-date-to-dac-in-real-time-on-ez-kit-sc589

    Best Regards,
    Santha kumari.K

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh

  • RE: ADP5091-1-EVALZ board

    Hi John,

    There may be a little confusion. You can see the equation of SETBK, SETSD and SETPG are same but TERM equation is different. So you can select the resistor from column 2 and 3 when you calculate the SETSD, SEBK or SETPG. Only for TERM, you need…

  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…

  • ADA4627-1 and ADA4637-1 Null Inputs Connection

    Hi,

    ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?

    Regards,

    Ivan.

  • 2 CVBS+1 LVDS input ->1 LVDS output ?

    Dears,

    Does ADI have the solution that support 2 CVBS and 1 LVDS(5 wires) input then 1 LVDS output?

    The CVBS signal is from camera and the  LVDS is from video or navigation.

    The output LVDS will display in 800x480/1024x600 screen.

    This is the siganal…