• 最爱ADI放大器-ADA4692-2

    最爱ADI放大器-ADA4692-2 by songchenping

    我们的变送器产品中用到放大器芯片对传感器探头信号进行预处理,因为是4...20mA接口,因此需要低功耗的放大器芯片。我们就选择了ADI的放大器ADA4692-2.

  • 最爱ADI放大器-ADA4692-2

    我们的变送器产品中用到放大器芯片对传感器探头信号进行预处理,因为是4...20mA接口,因此需要低功耗的放大器芯片。我们就选择了ADI的放大器ADA4692-2.

  • Voltage follower on ADA4692 cut of the signal

    I try to create simple voltage follower on ADA4692 but there was a surprise. In some reason it cut of the signal. In any follower shemes. I try all possible shemes. If I tied input to Vcc (3V) the output is still on cutt-of position (near 2V). Any other…

  • 4:4:4 encoding?

    Is there an Analog Devices part that can accept 4:4:4 encoding?

  • ADV7612 4:4:4 YCrCb

    Hi

    datasheet on page 13 states that the ADV7612 supports 36-bit 4:4:4 YCrCb, but the table 5 and 6 do not list this mode. Is it supported, how can it be activated?

    best regards


    Dani

  • av code section for 4:4:4

    I have a question. What is the content of Section AV for YCbCr 4:4:4 24 bit interface?

  • ADV7612 DDR 4:4:4 Output Modes data

    Page 13 of DS describes the PIXEL INPUT/OUTPUT FORMATTING The output section of the ADV7612 is highly flexible. The pixel output bus can support up to 36-bit 4:4:4 YCrCb or 36-bit 4:4:4 RGB. The pixel data supports both single and double data rates modes1…

  • ADV7619 4k 8bit 4/4/4 pass through

    Hello,

      I wanted to ask for clarification on the VS and HS signals with the ADV7619 in pass through mode.  i read the thread on this previously https://ez.analog.com/message/156902#156902 and it does say that the CP will be bypassed and the syncs remain…

  • ADV7627 RGB 4:4:4 Color Space Issue

    We are using the ADV7627.

    An error occurs when we have a source generating RGB 4:4:4. Output color is incorrect and exhibits lots of pink.  When the source is connected directly to the display everything looks just fine. BTW, auto-CSC doesn't seem to…

  • ADV7511 1080p RGB 4:4:4 script needed

    Could you please provide the IIC configuration script for ADV7511 HDMI

    I am working on the ADV7511 chip, which is the HDMI codec in VC707 EVB from

    FPGA company Xilinx.

    I want to configured the ADV7511 working in 1080P, 4:4:4 RGB input (each

    component…