• ADuM5401: Is 1 Mbps the maximum data rate, can this device be used above 1 Mbps?

    For the ADum5401ARWZ a Maximum Data Rate of 1 Mbps is given. Is this data rate
    a useful operating rate or is
    this the absolute maximum rate? what will happen to the signal above 1 Mbps?

     

    1 Mbps is the maximum data rate for the A grade ADuM5401…

  • ADM1186-1 channel

    Hi,

    About the 4 channels of ADM1186-1, I don't want to use the fourth channel.

    But I couldn't find the solution of this situation in datasheet.

    So, the 4th channel can be disabled? How to deal with the Pins:VIN4、OUT4、DLE_EN_OUT4 ?

    thanks!

  • Understanding LTC4008-1

    Dear community,
    I'm an engineer in charge of the development of a truck sensor testing device. Right now i'm tackling the battery management system. For that purpose, I'm using IC LTC4008-1, but I'm not sure I'm getting it to work properly.
    This is the…
  • AD5560XSVUZ-1

    Hello,

    1. Can I get a data sheet for AD5560XSVUZ-1?

    2. Can it be direct replaceable against AD5560JSVUZ?

    Thank you for your support.

    Best Regards,

    Herm Han

  • ADRV9008-1 malfunction

    Hello ADI team,

    I am working on several ADI cards such as ADRV9008-2, ADRV9008-1, ADMV1013-EVALZ, ADMV1014-EVALZ etc.
    I am very tired of the ADRV9008-1 reception card. Indeed, each time I load it by clicking on ''program'', it displays errors. I am obliged…

  • LTC6811-1 Voltage Measurement unprecise

    Hey together,

    we are working with the LTC6811-1 on an own PCB. The voltage values are read over I2C. We were able to implement nearly all features in our Microcontroller. Temperatures etc. are correct.

    But we have an issue with the voltage measurement…

  • RE: About LT6109-1

    Hi GEOFF123,

    Following page 16 on the datasheet and Figure 3. 
    I had this quick configuration on your scheme, if I got this right, 1.5A is your overcurrent trip and 0.05A is the under current. I assumed that your Imax is 2A for this config.

    The graph…

  • ADA4857-1 1 to 4 fanout

    Dear Sir/Madam,

    I am after some PCB routing advice on connecting one ADA4857-1(gain of 2) to four ADA4857-1 (gain of 1).
    The delay between the ADA4857-1 is not important just signal quality.

    Regards Joe

  • ADAQ7768-1 CRC

    Hello,

    I have enabled CRC Check (EN_SPI_CRC=1,CRC_TYPE=0)

    Then I use single-read mode from ADC_DATA. I received CRC but I think it is different than it should be.

    Eg.

    I receive data: 0xff 0xfb 0x47 (adc_buf[1],adc_buf[2], adc_buf[3])

    According to datasheet…

  • REQUEST TROUBLESHOOTING WITH LTC6804-1

    Hi BMS specialist,

    There is a delivery problem with ltc6803-3, so our customer is changed it to ltc6804-1 and designed a circuit and is testing it.

    Cell accuracy is being measured normally. However, when performing passive cell balancing, a channel with…