• RE: LTC6363-1 replacement LTC6363-1 replacement LTC6363-1 replacement

    Hi Mamzi,

    Have you checked on our authorized distributors? What package do you need?

    You can check Analog Devices' parametric search for single-ended to fully differential amplifiers

    Single-Ended to Differential Amplifiers Fixed Gain Selection

    Regards…

  • 2 ADAU1701 AND 1 1 I2C LINE

    Hello, there. The card I designed includes 2 ADAU1701, 3 tanae EEPROM and 1 processor. They are on the only I2C line to communicate with each other. I've made and run software for 1 Adau in the Sigma studio app. But 2. Adauya code is not going. The device…

  • what does the "-3" on the brand of ADV7390/1/2/3 and ADV7340/1/2/3 indicate?


    The latest revision of the encoder has the -3 version branded on it's package. The revision code of the encoder can be read back from register 0xBB bits 7:6. 01B indicates the latest revision.

    Further information on the change made to this version…

  • RE: HMC767: writing 1 to 02h (setting Reference Divider to 1) makes it so no SPI reads are correct

    Hi

    Indeed we have a 10 ohm series resistance on SPI lines. This helped fix communication issues due to glitches and reflections on the line.

    Regarding SPI mode selection on boot up, I don't think that's the issue here, as SPI communications are restored…

  • LTC3722-1

    can LTC3722-1 can be used for designing 6000W,200A isolated power supply

  • LTC3114-1 evaluation board SCP-LTC3114-1-EVALZ

    On the evaluation board for the LTC3114 Diode D2 connects to SW2 on the IC, What does it do, and under what conditions is it needed? We are supplying  12V at 1amp from 9 to 30V input to external customer supplied devices, these may have there own input…

  • ECG 12D ADAS : could i use 2 ADAS1000 (1 master 1 slave) instead of an ADAS1000-2

    Hi everyone,

    Because of the current component shortage, we are wondering if we can replace our ADAS1000-2 by a second ADAS1000 in order to get ECG 12D ? We tried to replace it by an ADAS1000 on an existing board but i can't get a frame from the slave…

  • ADuM5401: Is 1 Mbps the maximum data rate, can this device be used above 1 Mbps?

    For the ADum5401ARWZ a Maximum Data Rate of 1 Mbps is given. Is this data rate
    a useful operating rate or is
    this the absolute maximum rate? what will happen to the signal above 1 Mbps?

     

    1 Mbps is the maximum data rate for the A grade ADuM5401…

  • Understanding LTC4008-1

    Dear community,
    I'm an engineer in charge of the development of a truck sensor testing device. Right now i'm tackling the battery management system. For that purpose, I'm using IC LTC4008-1, but I'm not sure I'm getting it to work properly.
    This is the…
  • AD5560XSVUZ-1

    Hello,

    1. Can I get a data sheet for AD5560XSVUZ-1?

    2. Can it be direct replaceable against AD5560JSVUZ?

    Thank you for your support.

    Best Regards,

    Herm Han