• ADA4637-1 and OP37 pin compatibility in SOIC

    Are ADA4637-1 and OP37GSZ in SOIC package pin compatible?

     

    ADA4637-1 and OP37GSZ, are not pin compatible. But if you can externally short
    pin 5 and 8, then they become pin compatible.
  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…

  • ADA4637 OP Oscillate

    Hi,

    Have the below circuit with ADA4637, without or with input, have the below interesting issue.

           ----30M oscillation when C34 is 220pf, Oscillation disappear when C34 is 12pf. Why? Change R35 can't help.

          --I select other FET OP, there is similar…

  • ADA4627-1 and ADA4637-1 Null Inputs Connection

    Hi,

    ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?

    Regards,

    Ivan.

  • LTC3114IDHC-1#PBF & LTC3114IDHC-1#WPBF

    Dear Support,

    Good day,

    Please help me on the difference between part numbers below?

    What is the "W" meaning in the part number TC3114IDHC-1#WPBF?

     

    LTC3114IDHC-1#PBF

    LTC3114IDHC-1#WPBF

  • RE: Questions for LTC6811-1, LTC6812-1

    Dear Abhishek,

    Thank you for your kind answer.

    But additionaly my customer asks that they want to know the maximum power specification of Zennor diodes in LTC6812-1 and LTC6811-1.

    (Its zennor diodes are located inside of LTC6812-1 and LTC6811-1 and Cx…

  • Difference between LTC3114IDHC-1#PBF & LTC3114IDHC-1#WPBF

    Dear Support,

    Good day,

    Please help me on the difference between part numbers below?

    What is the "W" meaning in the part number TC3114IDHC-1#WPBF?

     

    LTC3114IDHC-1#PBF

    LTC3114IDHC-1#WPBF

     

  • LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF

    Could anyone explain what 3NS means on part numbers such as LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF ?

    I cannot find any information.

    thank you

  • "AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1) " is Valid?

    HI.

    I have a question about some code in BATImpedance.cpp.

    ------------------------

    AD5940_WriteReg(REG_AFE_SWMUX, 0);

    or 

    AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1);

    -----------------------

    In the datasheet REG_AFE_SWMUX  (0x0000235C)

    [2:0] reserved ,