Hi,
My customer is considering ADA 4627-1.
So I got a question.
What is the input voltage range and output voltage range
when ADA4627-1 is used with V + = + 5V and V- = -5V?
Best regards,
Yuya
Hi,
My customer is considering ADA 4627-1.
So I got a question.
What is the input voltage range and output voltage range
when ADA4627-1 is used with V + = + 5V and V- = -5V?
Best regards,
Yuya
Hi,
ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?
Regards,
Ivan.
使用±15V电源,为这两个芯片供电,焊接上这两个后电流明显增大,4627电流大概70mA,8253电流大概40mA.这是为什么呀?有哪个地方没有处理对吗?
Hi everybody,
I am currently trying to build a photodiode transimpedance amplifier based on the ADA4627-1 opamp. The first result I have obtained on a prototype circuit are quite bad, as I get a lot of excess noise generated inside the circuit.
I think…
Dear Support,
Good day,
Please help me on the difference between part numbers below?
What is the "W" meaning in the part number TC3114IDHC-1#WPBF?
LTC3114IDHC-1#PBF
LTC3114IDHC-1#WPBF
Dear Abhishek,
Thank you for your kind answer.
But additionaly my customer asks that they want to know the maximum power specification of Zennor diodes in LTC6812-1 and LTC6811-1.
(Its zennor diodes are located inside of LTC6812-1 and LTC6811-1 and Cx…