• ADA4941-1

    Hi All,
    I am looking for OPAMP which can convert single ended signal to differential signal to drive the ADC which has differential input. I have selected ADA4941-1 and tested for -2 and +2 gain configurations which are mentioned in Figure 58 and Figure…
  • LT3070 vs LT3070-1

    Dear Forum members.

    Could you please clarify what the difference is between the two devices?

    Thank you very much

    Regards

  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…

  • LTC3882-1 issue

    Hello,

    I ran into an issue using LTC3882-1 in our custom design. We are using LTC3882-1 together with UCD7242 to generate 1.0V core Vdd for LS1046A processor. Only channel 0 of LTC3882-1 is used, channel 1 was set to be off. I am trying to figure out…

  • Differential video transmission with ADA4433-1 and ADA4830-1

    Hello,


    Thanks for providing the spice model of both ADA4433-1 and the ADA4830(-1).

    I'm trying to design a DC coupled differential transmission system using the ADA4433-1 and the ADA4830.

    The overall gain from input (ADA4433-1) to output (ADA4830…

  • RE: HMC666_using IF pin without 1:1 transformer

    Hi Josh,

    IF port could be used as single ended but the conversion loss will be 3dB more than specified in datasheet, and the isolation maybe worse.

    Regards.

  • Powerful Combinations are Possible when 1+1>2

    It’s a new beginning for Analog Devices and Linear Technology. Together we become the high-performance analog industry leader with an innovation engine fueled by our comprehensive portfolio of analog and mixed signal products and solutions.

    We have…

  • How to configure 1 TX-1 RX in No-OS

    Hi all,

        My design uses ADFMCOMMS2 module and ZEDBOARD, I want to transmit data using 1 TX- 1 RX but the default set 2  TX-2RX in No-OS, so what parameters in  default_init_param in main.c file I need to modify in order to  set 1 TX- 1 RX, thank you for…

  • RE: ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hi katsu,

       The supply pins you mentioned above are still connected internally to the supplies of the ADATE305. They should still be shorted to VDD and VSS respectively. The reason for their special mention on the datasheet was so the user can pay special…

  • What the difference between the ADA4940-1 and the ADA4941-1?

    What is the difference between the ADA4940-1 and the ADA4941-1? They are both ADC drivers, but what distinguishes the two parts from each other?