Q1. What is the ADA4622-4 / ADA4622-2 / ADA4622-1?
A1. The ADA4622-4 / ADA4622-2 / ADA4622-1 is the next generation of the AD824 / AD822 / AD820. It is a single supply, 30 V, 8 MHz, Low Bias Current, Single-Supply, RRO, Precision JFET Op Amp.
…
Q1. What is the ADA4622-4 / ADA4622-2 / ADA4622-1?
A1. The ADA4622-4 / ADA4622-2 / ADA4622-1 is the next generation of the AD824 / AD822 / AD820. It is a single supply, 30 V, 8 MHz, Low Bias Current, Single-Supply, RRO, Precision JFET Op Amp.
…
Hi,
I need some help.
As below picture picked from the datasheet.
https://www.analog.com/media/en/technical-documentation/data-sheets/ada4622-1-4622-2-4622-4.pdf
The EPAD of 2ch Version(ADA4622-2) is recommended to connect the EPAD to V+, but the note…
I read Datasheet of ADA4622-1/ADA4622-2(Rev. B).
I have a question.
The ADA4622-1/ADA4622-2 are the next generation of the AD820 and the AD822 single-supply, rail-to-rail output (RRO),precision junction field effect transistors (JFET) input op amps…
Hi,
May I know how much current/voltage are you anticipating at the input of the ADA4622-2?
You could refer to page 28 of the datasheet for some guide regarding input protection of the ADA4622-2
Thanks,
Donnie
Hi Zayouna,
An alternative to ADA4622-2 could be the ADA4610-2 which has lower 1/f noise (0.45uApp), 16.3MHz GBWP, 25 V/us SR, 10^13 ohm input resistance. The "Vos TC" (offset drift) of ADA4610-2 (2uV/deg. C, B Grade) is better than ADA4622-2…
I read Datasheet of ADA4622-1/ADA4622-2/ADA4622-4(Rev. D).
I have a question.
IN ELECTRICAL CHARACTERISTICS, VSY = ±15 V Current Noise Density is 0.8fA/√Hz. (Rev. D | Page 4 of 37)
I See.
IN ELECTRICAL CHARACTERISTICS, VSY = ±5 V
…In the Page 1 of the specsheet, the final paragraph reads:
The ADA4622-1 is available in a 5-lead SOT-23 package and an 8-lead LFCSP package
while in the Page 11 of the specsheet, the page shows:
Figure 2 and Figure 3, showing the ADA4622-1 in the SOT…
Hi, I am interested in ADA4622-4 opamp grade B but this grade seems not to be available in the 4 opamp package. It is correct?
Thank you in advance
I'm curious about the shutdown/disable feature of the ADA4622-1.
What is the impedance looking into the ADA4622-1 at its inputs and output when the part is in shutdown? I like the idea of a circuit like Figure 99 of the datasheet, but what extra load…
I was wondering what the electrical differences were between the LFCSP and SOIC_N packages on the ADA4622-4. The size of the LFCSP package is elegant, but it also has an EPAD on it which should help with heat dissipation, right? Are there any other measurable…