Any suggestion for a beteer alternative for ADA4622-2
Have equal or better 1/f noise, bandwidth >5MHZ, slew rate, input impedance >10^9, high slew rate.
Any suggestions?
Thanks
Zayouna
Any suggestion for a beteer alternative for ADA4622-2
Have equal or better 1/f noise, bandwidth >5MHZ, slew rate, input impedance >10^9, high slew rate.
Any suggestions?
Thanks
Zayouna
ADA4622: it is recommende to connect the epad to V+. But can it be connected to any other signal such as GND? Why V+ any specific reason for that?
Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:
[Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
.file_attr 1="1";
syntax error is at or near text '1'.…
Greetings!
I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…
|
Hello,
In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?
Best Regards,
Hello Team.
1:1 transformer applied in IF pin is expensive.
so we want to use without transformer.
is it possible that?
Can you support solutions?
thanks.
Best regards,
Josh
I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…