• RE: Looking for DAC with EEPROM / Flash

    Hi Ramakrishna,

    Since we do not have a DAC with EEPROM, i would suggest using AD5292 digipot along with a ADA4610-1 amplifier in buffer configuration to achieve your objective. 

    Regards,

    Koushik

  • RE: AD711 - Floating Null Pins

    Hi John,

    You're welcome!

    Other op amp that is worth considering is ADA4610-1. It has higher speed, lower noise, lower bias current and lower current, RRO with better drift.

    Regards,

    Phil

  • RE: transimpedance amplifier

    FormerMember
    FormerMember

    Nisha,

      Take a look at the newer ADA4610-2.

    Harry

  • ADA4610 Single Supply

    Using ADA4610 for color light diode sensor ... prefer to use just a single +5V supply vs the +/- 5V supplies.  Any notes on the successful hookup?  Issues that may be expected?

  • What other Jfet amplifier can replace ADA4610? I cannot find it on supplier sites anymore. Thank you!

    What other Jfet amplifier can replace ADA4610? I cannot find it on supplier sites anymore. Thank you!

  • RE: anveshan 2015080: AD8606 is getting heated up

    Hi Koushik,

    How is your circuit coming along so far? I think it would be easy for you to just maintain your original schematic and replace the AD8606 parts with any one of these: ADA4610-2 (Dual), ADA4610-4(Quad) and ADA4000-4(Quad). These parts really…

  • RE: ADA4610 fitted for Sample&Hold  ?  Bandwith 2-22kHz, signals up to 6Vpp, Supply 2x 12V, Hold cap 120pF

    Hello Kris.

    Thanks a lot for your opinion.

    I can count on the ada4610 and your advise.

    Met vriendelijke groet,

    Hans Splinter, TS Solar Nederland.

    ( Vanaf mijn mobiele telefoon ).

    Op 30 nov. 2017 om 13:23 heeft krisf <analog@analog-vm.hosted.jivesoftware…

  • EV-AD5415/49SDZ 輸出電壓調整35V

    EV-AD5415/49SDZ 關於這板子是否可以變更為輸出電壓為35V

    可有建議的OP,我自己挑了一個ADA4610-2ARZ 不知道可以不可行


    另外在AD5415 若搭配ADA4610有甚麼地方要注意的 ?

  • RE: AFE for AD7768-4

    Hi,

    The most suitable front-end amplifiers for this type of application are amplifiers like the ADA4610-1, ADA4610-2, or AD8605, AD8606. These amplifiers provide a low noise option which makes them suitable for use in signal chains using low noise ADC…