• ADA4571 Temperature data

    Hi every one. From data sheet, for converting raw data to 'C, I can't understand what is "TCvtemp" parameter.  

    So, what is "TC" value?

    Thanks.

  • RE: Choose a variable gain amplifier for hall effect sensor output

    Hello again Hank, 

    One more option for you -- are you set on using a Hall effect sensor? You could also use an AMR sensor for your application. The ADA4571 has an integrated sensor and conditioning circuit and is suitable for position sensing. I highly…

  • Downloading the SDP driver via FTP does not work for me

    I just tried to download the SDP driver via ftp.

    Unfortunately, that wasn't possible.

    Can you send me the driver; I need to test the ADA4571 and I am a little under pressure!

    Thanks

    Christian

  • ADA4571 for PMSM motorcontrol sine commutation

    Hello,

    i have an ADA4571 GMR-Sensor with a 30 pole Magnetring (Off-Shaft integartion). The sensor works very well and the estimated angle is very accurate, but my question is, can i obtain a 360° mechanical angle with this build? I know that the ADA4571…

  • ADA4571软硬件连接时提示检测不到daughterboard,各位怎么看?

    刚刚试用ADA4571,电脑上软件安装好了,2块硬件板子也接好了,但是按照软件提示进行连接时,却提示检测不到daughterboard,见附件。试了好多次都不行,只好请大家帮忙分析一下了,谢谢~~

  • 最新中文资料更新(2015年3月)

    中文数据手册

     

     

    应用笔记

     

    AN-897

    AN-793

     

    参考设计

     

    基于ADSP-CM408的电机控制系统

     

    技术文章

     

    MS-2739

    MS-2773

  • RE: ADA 4571 Phase Shift Problem

    Thank you for your interest in the ADA4571 and for posting your question in the EngineerZone.  We do not actually support this product in this particular forum, but I will find out which forum this belongs in and move this discussion to that forum, so…

  • RE: Is there a replacement for the IPA 1751 Inductosyn Preamp IC

    Hi Jason, 

    As this device is very old, we do not have any direct drop-in replacements. However, these reference circuits may be of help:

    CN0368 - uses the ADA4571 AMR with integrated signal conditioning

    CN0301 - uses the AD698 LVDT signal conditioner

  • ADA4517

    Hi every one. The output of ADA4517 is in degree or radian? (a=atan(vsin/vcos)/2)

    How to test this sensor?

    Thanks.

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…