• RE: .file_attr 1="1";

    Hi Gideon,

    I moved this thread to the "CrossCore Embedded Studio and Add-ins" forum as it appears a tools related issue.

    I suspect that one of the automatic file attributes is being replaced by a macro define in the compiler generated assembly…

  • LTC6813-1

    Application Question for LTC6813 and similar parts.  Using the cell balancing capability of these devices is not required, is it?  If not, what do you do with the unused pins?

    Additionally, I plan to use the part to measure a string of 12V VRLA batteries;…

  • LTC3721-1 ΘJc

    Hi,

    I'm considering the LTC3721EGN-1,
    Is there data on ΘJc for this IC?

    Best regards,

    Yuya

  • LTspice ADHV4702-1

    你好,

    我需要輸出+-60V/1Aout的1KHz Sine wave,所以選了ADHV4702-1加上LT1166來模擬,發現在一開始的時候,輸出端有個pulse出現,

    於是參考ADHV4702-1 datasheet內的TYPICAL APPLICATION CIRCUIT 模擬,但是輸出總是會有一個pulse出現.

    於是改成Unity-Gain Buffer,並且輸入端下地,依然輸出有一個pulse出現.

    請問該如何解掉這根pulse呢?謝謝.

  • LTC6810-1

    Application Question for LTC6810 and similar parts.  It's not required to use the discharge capability of these devices is it?  If not, what do you do with the unused pins.  I didn't see anything in the data sheet pertaining to this question. 

    Additionally…

  • RE: Powering LTC6813-1

    For this application you can use LTC6806 instead of LTC6813

  • LTC3108-1

    Hi,

    We are working on PoC based on LTC3108-1. We wish add a LED for visual monitoring, LTC3108 is not able to supply a suffisient current to drive the LED.

    Could we use C2 input for drive an external Mosfet (low Qg) ?

    BR

    Benjamin

  • RE: TCXO with ADF7020-1

    Hi Kosta,

    A TCXO reference can also be used for the ADF7020-1. This is mentioned in page 15 of the datasheet under the Reference Input subsection, "A single-ended reference (TCXO, CXO) can also be used"

    Regards,

    Aldrich

  • AD9523-1 setting with AD9523

    Hi,

    Our customer used AD9523 before. But AD9523 NRND, they need to change to AD9523-1.

    1. If they change to AD9523-1, do they need to modify the firmware or hardware?

    2. AD9523-1 add VCO Divider M1 and M2 Coupling meanwhile add some register.
    Could you share…