• ADA4505 - Minimum output series resistor

    For op-amp type AD4505 what is the minimum output series resistor value necessary to drive any output capacitance.

    The loop gain set by feed back will be low - for example unity gain follower, or DC gain of 20 and low AC gain set by a feedback capacitor…

  • ADA4505 & AD8500 noise density vs frequency

    Hi

    Can you share the raw data of AD8500 and ADA4505 voltage noise density vs frequency chart?

    (Figure 24 of AD8500 datasheet and Figure 36 of ADA4505 datahseet)

    I'm building front end circiut using those parts and need those data for computing RMS…

  • 4:4:4 encoding?

    Is there an Analog Devices part that can accept 4:4:4 encoding?

  • ADV7612 4:4:4 YCrCb

    Hi

    datasheet on page 13 states that the ADV7612 supports 36-bit 4:4:4 YCrCb, but the table 5 and 6 do not list this mode. Is it supported, how can it be activated?

    best regards


    Dani

  • av code section for 4:4:4

    I have a question. What is the content of Section AV for YCbCr 4:4:4 24 bit interface?

  • ADV7612 DDR 4:4:4 Output Modes data

    Page 13 of DS describes the PIXEL INPUT/OUTPUT FORMATTING The output section of the ADV7612 is highly flexible. The pixel output bus can support up to 36-bit 4:4:4 YCrCb or 36-bit 4:4:4 RGB. The pixel data supports both single and double data rates modes1…

  • ADV7619 4k 8bit 4/4/4 pass through

    Hello,

      I wanted to ask for clarification on the VS and HS signals with the ADV7619 in pass through mode.  i read the thread on this previously https://ez.analog.com/message/156902#156902 and it does say that the CP will be bypassed and the syncs remain…

  • ADV7627 RGB 4:4:4 Color Space Issue

    We are using the ADV7627.

    An error occurs when we have a source generating RGB 4:4:4. Output color is incorrect and exhibits lots of pink.  When the source is connected directly to the display everything looks just fine. BTW, auto-CSC doesn't seem to…

  • ADV7511 1080p RGB 4:4:4 script needed

    Could you please provide the IIC configuration script for ADV7511 HDMI

    I am working on the ADV7511 chip, which is the HDMI codec in VC707 EVB from

    FPGA company Xilinx.

    I want to configured the ADV7511 working in 1080P, 4:4:4 RGB input (each

    component…

  • ADV7625 RGB 4:4:4 Color Space Issue

    I started this question with my original post: ADV7627 RGB 4:4:4 Color Space Issue 

    Colorspace continues to plague my system and I am looking for some guidance. I have spent a considerable amount of time looking at the AVIAPI routines but there are some…