• RE: ADA4505 & AD8500 noise density vs frequency

    Hi, In.

    I had attached the raw data of the noise density vs frequency graph of ADA4505-1. I'll get back to you once I have the data for AD8500.

    Regards,

    Anna

  • ADA4505 - Minimum output series resistor

    For op-amp type AD4505 what is the minimum output series resistor value necessary to drive any output capacitance.

    The loop gain set by feed back will be low - for example unity gain follower, or DC gain of 20 and low AC gain set by a feedback capacitor…

  • ADA4857-1 1 to 4 fanout

    Dear Sir/Madam,

    I am after some PCB routing advice on connecting one ADA4857-1(gain of 2) to four ADA4857-1 (gain of 1).
    The delay between the ADA4857-1 is not important just signal quality.

    Regards Joe

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • RE: 请问ADIS16495-1和ADIS16505-1,如何直接连接windows 10 pc使用呢。

    我们有相应的开发板和Windows版软件,在对应芯片下面都可以找到

  • ADA4700-1供电

    ADA4700-1手册写的是双电源供电,能单电源供电吗

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh