• Input Voltage Range of ADA4433-1W.

    Hello.

    I have some questions about ADA4433-1W.

    Question 1.
    I think minus voltage level can not input to Vin+, Vin-.
    Is this right?

    Question 2.
    On datasheet P.4, there are following descriptions:

    INPUT CHARACTERISTICS
    Input Common-Mode Voltage Rang…

  • ADV7390/1 with the video in double image

    Dear FAE

          When using the ADV7390/1 in the 360 surround view application, I.Max6+ADV7390+ADA4433-1 with the CVBS output. But showing in the LCD , found the the video is in double image.

           Having checked the video source, it is OK.

           Cloud you help to…

  • Full-HD Composite Video Filter Driver

    Hello,

    My customer has been looking for Full-HD Composite Video Filter Driver.
    For example, the competitor is "TPF140".

    http://www.3peakic.com.cn/resources/download/TPF140.pdf

    Does ADI have any Full-HD video driver/filter like "TPF140"?…

  • Require Baking condition

    Can you please share the baking condition for the below mentioned parts.

    Item MFG Part Part Description
    1 ADP3300ARTZ-3-RL7 IC REG LDO 3V 50MA SOT23-6
    2 ADA4412-3ARQZ IC FILTER…
  • Diagnostic Technique Detects Open and Short Circuits in Wiring Harnesses

    Did you know that the wiring harness in most modern automobiles is the second most costly item, first only by the powertrain?  Diagnosing cable faults in automotive applications then becomes a very important function to help reduce cost and save time…

  • LTC3108-1

    Hi,

    We are working on PoC based on LTC3108-1. We wish add a LED for visual monitoring, LTC3108 is not able to supply a suffisient current to drive the LED.

    Could we use C2 input for drive an external Mosfet (low Qg) ?

    BR

    Benjamin

  • RE: .file_attr 1="1";

    Hi Gideon,

    Sorry for the delay in responding.

    The cause of the problem is "-file-attr CORE0" and "-DCORE0" both being included on the compiler command-line. Could you delete CORE0 from the "Additional attributes" in Tools Settings > CrossCore Blackfin…

  • RE: (Video decoder)Full differential connect

    1) In the figures above, ignore all the components past the 1.3KOhm resistor.  They have very little affect on the impedance calculation.

    1a) Figure 45.  Keep in mind the ADA4433 has a 2x gain.  If you are using the ADV4433 then follow the data sheet Figure…

  • LTC2942-1

    Hi.

    The Sense+ pin is connected to both Charger and Load. So,I would like to know how the LTC2942 could determine the operation mode between charge and discharge.

    Thanks.

  • Bidirectional switch with LTC7000-1

    Dear community,

    I would like to design a bidirectional switch allowing current to flow in both directions, like a relay. I want the solution to control MOSFET's power dissipation in order to stay in their SOA. The voltage will be 15V min, 55V nominal…