• RE: ADA4432-1 and AD7393

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADA4432-1 IC as a video receiver amplifier

    Poornima,

    I think you have misunderstood my question. I'm using ADA4432-1 at the output of video DAC(ADV7393) as driver. My question is can I use the same IC ie. ADA4432 as receiver buffer/filter for PAL video signals?

  • RE: ADV7391 High Drive Compensation Pin Connection

    Dear Joseph

    Please find the below link for ADA4432-1/ADA4433-1 component datasheet.

    http://www.analog.com/static/imported-files/data_sheets/ADA4432-1_4433-1.pdf

    Please refer to figure 53 which uses ADV7391 component, in which COMP pin is connected…

  • RE: Video out from AD7341

    Hi,

    For a composite video amplifier with a shutdown feature the ADA4430-1 and the
    ADA4432-1 are good options.

     

    Regards,

    Paul

  • ADA4432-1 output short to 24V battery test protection

    Hello,

    My customer used ADV7391+ADA4432-1 as CN0264. It is work fine with 12V battery short protection test.

    As project will extend to Truck application, the battery capability will be 24V.

    Is ADI any suggestion or experience sharing for this kind…

  • Part Obsolescence Query

    Hello,

    We are using the following ADA parts in our design and would like to know what is the expected time to being obsolete.

    1. ADA4432-1BCPZ-R2

    2. ADV7182WBCPZ

    3. ADA4830-2BCPZ-R7

    Please let us know as soon as possible.

    Thank you,

    Jayesh Tanwan…

  • (ADA4432)To make Pseudo Differential output

    Hi !

    Our customer want to input Pseudo Differential CVBS to ADV7281A-M but they don't have the video source.

    So they are thinking to make Pseudo Differential signal from single CVBS video source.

    I was reading ADA4432's datasheet.

    I understood…

  • RE: ADA4432 Reflow profile

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADA4433 short Output to GND

    Hi Goz,

    It's application is automotive camera module. 

    Customer use ADA4432 for single-end but they want to use ADA4433 to improve EMC by using differential signal. 

     

    Thanks very much!

     

    Henry