• What are the tresholds for the ADA4431-1 "load detect" function ?

    The nominal load for the ADA4431-1 is 75 Ohms.

    But what are the min and max tresholds for the ADA4431-1 "load detect" function ?

  • ADA4431-1 Negative Sync Level

    Hi,

    Doing some final checks on the negative sync level of the ADA4431-1 in our circuit, attached as shown.  With a 75 ohm resistive load on the output, the sync level is -180mV, and not near -300mV.  I am unsure why and am looking for help.  With the load…

  • LTC3114IDHC-1#PBF & LTC3114IDHC-1#WPBF

    Dear Support,

    Good day,

    Please help me on the difference between part numbers below?

    What is the "W" meaning in the part number TC3114IDHC-1#WPBF?

     

    LTC3114IDHC-1#PBF

    LTC3114IDHC-1#WPBF

  • RE: Questions for LTC6811-1, LTC6812-1

    Dear Abhishek,

    Thank you for your kind answer.

    But additionaly my customer asks that they want to know the maximum power specification of Zennor diodes in LTC6812-1 and LTC6811-1.

    (Its zennor diodes are located inside of LTC6812-1 and LTC6811-1 and Cx…

  • Difference between LTC3114IDHC-1#PBF & LTC3114IDHC-1#WPBF

    Dear Support,

    Good day,

    Please help me on the difference between part numbers below?

    What is the "W" meaning in the part number TC3114IDHC-1#WPBF?

     

    LTC3114IDHC-1#PBF

    LTC3114IDHC-1#WPBF

     

  • LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF

    Could anyone explain what 3NS means on part numbers such as LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF ?

    I cannot find any information.

    thank you

  • "AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1) " is Valid?

    HI.

    I have a question about some code in BATImpedance.cpp.

    ------------------------

    AD5940_WriteReg(REG_AFE_SWMUX, 0);

    or 

    AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1);

    -----------------------

    In the datasheet REG_AFE_SWMUX  (0x0000235C)

    [2:0] reserved , 

  • RE: LTC6363-1 replacement LTC6363-1 replacement LTC6363-1 replacement

    Hi Mamzi,

    Have you checked on our authorized distributors? What package do you need?

    You can check Analog Devices' parametric search for single-ended to fully differential amplifiers

    Single-Ended to Differential Amplifiers Fixed Gain Selection

    Regards…

  • 请问型号AD5592RBCBZ-1-RL7中的-1是对应什么特别的信息?

    你好技术支持,

    想请教一个简单的型号问题,AD5592RBCBZ-1-RL7和AD5592RBCBZ-RL7之间有什么区别呢?

    我看了规格书,整个规格书都是将AD5592R和AD5592R-1并提,用或的符号“/”分开

    所以想请教下,这两个产品可以互相替换使用吗?

    另外,想问一下,一般ADI的规格书不会列出型号每个部分的详细解释,只会列出不同型号对应的部分功能,而且部分参数功能经常是一样的,像前面两个型号,在这个列表里像是完全是同样的产品

    遇到不同的型号怎么判断能不能替换使用…

  • 2 ADAU1701 AND 1 1 I2C LINE

    Hello, there. The card I designed includes 2 ADAU1701, 3 tanae EEPROM and 1 processor. They are on the only I2C line to communicate with each other. I've made and run software for 1 Adau in the Sigma studio app. But 2. Adauya code is not going. The device…