• RE: ADA4350 SWITCHING NOISE

    Hi,

    This concern is answered by Kelvin Switching Technique and is further discuss on page 27 of the data sheet.

    Thanks and regards!

  • RE: Maximum Input Current for ADA4350?

    Hi,

    I would agree with you that feedback R has a role that will affect the input current and output voltage.
    In general, you would set the feedback R such that the maximum attainable output voltage corresponds to the maximum input current allowing the…

  • ADA4350: LTSpice Simulation

    Hi,

    I'm having difficulty setting up the spice simulation for the ADA4350 in LTSpice. So far I have downloaded the ADA4350.cir file through the site and have created a symbol for the ADA4350. How do I link the .cir file to the part itself?

    Thanks…

  • ADA4350 driving LTC2380

    We need ADIs valuable suggestion for the reference voltage to apply in the ADC driver in ADA4350 and its compatibility to LTC2380.  

  • ADA4350: On-Resistance

    Hello,

    I will connect the SWA_OUT pin of ADA4350 with an outside inverting amplifier circuit.

    I do not use the ADC DRIVER of ADA4350.

    The ADA4350 has the switch, and the on-resistance is hundreds of ohms.

    I think that the on-resistance is too large…

  • ADA4350 drive AD9650

    I'm using the ADA4350 to drive the AD9650. The front-end circuit of AD9650 is shown below. The sample rate is 20MHz.

    When I input a 100KHz sine wave to the ADA4350, The sample data is a stepped sine waves when ploted.

    I have another PCB of AD9650…

  • ADA4350 drive AD9650

    I'm using the ADA4350 to drive the AD9650. The front-end circuit of AD9650 is shown below. The sample rate is 20MHz.

      

    When I input a 100KHz sine wave to the ADA4350, The sample data is a stepped sine waves when ploted.

    I have another PCB of AD9650…

  • About ADA4350

    Hi

    I have a question ADA4350.

    I using S0,S1,S2. no using S3,S4,S5.

    6pin FB3,5pin FB4,4pin FB5 and 1pin SWB OUT is connect to GND .it is no problem?

    And ,

    When using ADA4350 and ADC, Is it no problem to change using chip select?

    Best Regards

  • ADA4350 SPI

    Can several ADA4350 devices be daisy chained together, with  SDO of one device connected to the SDI of the next one?

  • ADA4350 application

    This is my design circuit about ADA4350.

    Who can help me to check it ?

    The Power VSS=10V, VDD=5V.

    Single end signal input.

    Many thanks.