• Inquiry on output current spec(limit) of ADA4311-1

    Hi,

    We are considering design to PLC line driver application using ADA4311-1.

    The current competitor is TI OPA2673, which has an output current specification of 700mA(800mA limit)..

    I am curious about the exact output current specification of the ADA4311…

  • ADA4311

    I was designing a signal generator for gain control(the signal frequence is 2MHz to 30MHz).I am using ADA-4311 opamps,which terminates with a 50 ohm resistor in my design.The maximum input voltage is 2vp-p and power support is 12v.
    I would like to know…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • RE: About supply voltage of ADA 4310-1 (II)

    Hi Mochi,

    Apologies for the late reply. For your question if ADA4310-1 equivalent to the absolute maximum rating of ADA4311-1. The answer is no. Absolute values for the parts are ± 5% of 12V supply voltage for ADA4310-1 and 13.6V supply voltage for ADA4311…

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh

  • RE: LTC3300-1 Erase Schematic

    Hi Damon,

    This is ok now.

    Please clear your browser cache. If you search for MMBZ27CD in Google Search, result will redirect to ez.analog.com and PDF is no longer downloadable.