I have read the ADA4310-1 data sheet.
Is the input power supply voltage different depending on the package?Why is that?
Is it not allowed to use between 0 V and 12 V using the 16-Lead LFCSP package?
Best regards;
When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive…
Hi there,
I have some questions about ADA4310.
First, what is the absolute maximum voltage for INpin ,OUTpin and PD0/1pin?
Second, do you have a spec about the period from Power down mode to Normal mode by controlling PD0/1?
Thanks in advance.
Best…
Hello
My customer will use ADA4310 and is designing his cirucit.
Then he would like to get input impedance of ADA4310 for designing front end ( around signal source ) of ADA4310.
Datasheet P4 says below.
Input Resistance f < 100 kHz , Typ 500…
Hi Terumasa,
The documents available for this parts is only its datasheets which you can found on this product page: http://www.analog.com/en/broadband-products/broadband-amplifiers/ada4310-1/products/product.html
Let me know if you get any additional…
I have read the ADA4310-1 data sheet.(Rev. B) Operating Range (Single Supply): +5 to +12 [V]ABSOLUTE MAXIMUM RATINGS Supply Voltage: 12V Is it not recommended to use a 12 V (± 3%) power supply connected?Or is it either a mistake? Best regards;
I asked a question about this matter once. https://ez.analog.com/thread/98682Please allow me to ask you again.
Operating Range (Single Supply): +5 to +12 [V]ABSOLUTE MAXIMUM RATINGS Supply Voltage: 12V
I have confirmed that you can use ± 3% of your 12V…
Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:
[Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in : .file_attr 1="1"; syntax error is at or near text '1'.…
Greetings!
I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…
I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…