• RE: ADA4304-4

    Hi Show,

    May I know your application? You may want to check this article: https://www.analog.com/en/technical-articles/data-sheet-intricacies-absolute-maximum-ratings-and-thermal-resistances.html. This article discusses data sheet intricacies specifically…

  • ADA4304-4 Question

    In our product design, we use the ADA4304-4 chip to distribute the rf signal of cable digital TV, the 1 input of the rf signal is allocated to 4, in order to avoid the
    high-voltage electrostatic and leakage from rf signal input,we use a blocking capacitor…

  • 16 bit RGB 4:4:4 to pal

    I would like to ask any idea of IC that supports the conversion of digital RGB (16bit or 8bit) to analog PAL

  • RE: External reference connection to AD7380-4, AD7381-4, AD7389-4

    Hi Michael_kwe,

        In AD7381-4, an external reference can be used and a voltage reference must be driven into the REFIO pin. It is recommended to set the REFSEL setting correctly for proper device operation. When using external reference voltage, REFSEL…

  • On EVAL-CN0313 there are three different circuits that offer various protection levels for IEC61000-4-2 ESD, IEC61000-4-4 EFT and IEC61000-4-5 Surge. Why is there different protection circuitry used for Surge Level 4 compared ESD/EFT level 4?

    The EVAL-CN0313SDPZ is a certified EMC Compliant RS-485 Interface Design Tool. 

    The main reason for the different protection circuitry is related to the difference in energy levels associated with each of the transient waveforms. According to the IEC61000…

  • AD8307 4-pole low pass filter 32 / 5,000 Translation results AD8307 4-pole low pass filter design

    AD8307 Datasheet page 20 shows a 4-pole low pass filter design. As far as I know it seems to be a sallen-key topology.

    The datasheet states that changing the capacitors of C5~C7 will change the cut-off frequency.

    But in reality, it seems that the cut…

  • ADA4304-2

    Здравствуйте. Можно ли использовать микросхему ADA4304-2 для разветвления RGB или S-Video сигналов?

  • RE: Video splitter ADA4304-3

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: 4*4 Tx/Rx Beamformer

    External LO has a divide by 2 inside. This divide by 2 is random, and it's randomness is determined by the LO input power. (if LO goes away, and comes back, then the phase of the divide by 2 is random). This randomness also depends on power up cycles…

  • Video RF Splitters of ADA4304-2.

    Hi 

    We want to using the ADA4304-2.

    but we need to check these guideline data and want to follow reference design.

    include schematic ,Layout, s-parameter.

    Thank you!