Hi.
I have a board with ADV7611, and the output video must be in 4:2:2 format.
However the input video can be 4:2:2 and 4:4:4.
In ADV7611 Reference Manual, in page 86 said:
For a 4:4:4 HDMI input stream to the ADV7611
The DPP section filters…
Hi,
I have received a question at ADF4360-2 from the customer that, "By using devide-by-2 option for 2GHz VCO output, does it result to output 1GHz of 50% duty ?"
He said he is now having external discrete components of 1/2 dividing for VCO…
My question is if It´s possible to connect a load cell (+10VDC supply) with zero drift amplifier ADA4528-2 (+5VDC supply) for driving diferential input of AD7172-2 AD converter.
You can see the schematic attached.
regards.
ADV7619 HW User Guide (UG-237), Pg 27 lists PIXEL PORT OUTPUT MODES. I am interested in setting 0x8d for 20-bit SDR 4:2:2 Mode 3. The tables in Appendix C doesn't list setting 0x8d. Would it be similar to 0x81 which is on pg 199, Table 77, col…
We are using ADV7180 interfacing with i.MX27 processor.we are able to configure properly I2C bus,but incorrect YUV 4:2:2 video is coming from ADV7180 output.please help.
Hello.
This is my first post here.
I want to measure two loads, both are connected to the same 230v line. Can I use a shunt for load 1 and another shunt for load 2?. Is it possible with ADE 7953 using channel A and Channel B?
Best regards.
I recently bought the ADA4857-2 high speed opamp and the bare-board that allows me to prototype various circuits using the opamp. I want to create a circuit that converts the differential output coming from LTC5586 Zero IF IQ Demod board that I have…
I want to use the ADV7842 in YCbCr 4:2:2 16-bit SDR output mode with an input of either HDMI, YPbPr or Computer graphics. It appears this should be possible. I am trying to verify the hardware configuration for the P0 - P35 pins. What are the correct…
Hello,
We are using the ADV7619 in 4:2:2 16-bit mode output and we came across some kind of chroma subsampling issue.
The ADV7619 is working at 1080p60 with a RGB-FULL computer source and here are some screenshots taken from our board while using a…