Hi,
I have the EVAL-ADV7612-7511p video evaluation board .I'm using 7612 to receive HDMI inputs from camera(720p @60) , and then feed to 7511 to output the video to the screen.
camera -> 7612 --> 7511 --> screen
When adv7612 output 4:4:4 8bit ycrcb…
Hello
Thanks in advance.
I have a input video signal whose format is: YCbCr (Digital YUV) 20 bit (10 chroma + 10 luma).. 1080p60 (1920x1080 60 fps).
As I can read in this forum ADV7610 only supports four modes for SDR 4:2:2:
- 8 bit SDR ITU-R BT.656…
When I input YCbCr 4:2:2/12 into my ADV7619 and readi back 0x0B(DEEP_COLOR_MODE) of the HDMI map it always reports 8 bits per channel. I also see this on the eval board as well. While YCbCr 4:2:2/10 is reported correctly.
Is there some conversion in…
The windows application auto calculates the negative bleed current, even if FRAC1 and FRAC2 are not 0, but from the ADF4355-2 Rev C page 25, :
"Use negative bleed only when operating in fractional-N mode,that is, FRAC1 = FRAC2 = 0. Do not use negative…
请问这三款除了引脚不一样,集成运放数量不一样,4897带了使能端之外,4896与4897的性能是否一致?
Hi
I want to know ADV7623 Support Video Format.
ADV7623 support 4K/30p 4:2:2?
ADV7623 TDMS Frequency:225MHz.
So,I think ADV7623 support 4K/30p 4:2:2.
Did anyone use 4K/30p 4:2:2 at ADV7623 Eva Board?
Best Regards.
Take
I'm trying to connect with 2 jtags to 2 processors , BF547 and BF512, at the same time with no succes.
I have no Problem to connect to each one of them separatly.
I know that it's Posible to connect to 2 processors at the same time .
Do you…
在设计中采用AD7865 4通道ADC采集数据,由于采购问题,第一次采购的了AD7865AS-2,
第二次采购回来的是 AD7865asz-2. 通过数据手册查看到二者没有区别,但是在使用中对于同样的
情况采集回来的数据有大概4倍的差异,请问是正常的,还是有什么地方需要注意的?
以下数据为对某4个通道采样后的量化数据(二者工作的状态相同,工作电压和硬件电路相同):
AD7865AS-2 AD7865ASZ-2
8196 2049
9347 2348
10680 2677
Apologies for confusion. The above scenario is assuming that the part is operating with a single supply. There are two input voltage range to look at for most of the lower bandwidth Sigma Delta ADCs. First is the absolute input voltage range (per…
hi all,
Please reslove this..
i am using ADV76111 HDMI receiver.. and connecting it to SH7724.
We are connecting P[15:8] pins of ADV7611 to SH7724.
Which option is required to set YCbCr(4:2:2) 8-bit output on P[15:8]?
Options to set video are…