Здравствуйте. Можно ли использовать микросхему ADA4304-2 для разветвления RGB или S-Video сигналов?
Hi,
The ADA4304-2 can be used buffer video signals
Please refer below product page for ADA4304-2 Splitter
http://www.analog.com/en/products/amplifiers/specialty-amplifiers/video-rf-splitters/ada4304-2.html#product-overview
Thanks,
Poornima
In our product design, we use the ADA4304-4 chip to distribute the rf signal of cable digital TV, the 1 input of the rf signal is allocated to 4, in order to avoid thehigh-voltage electrostatic and leakage from rf signal input,we use a blocking capacitor…
Hello the ADA4304-3 can work as composite video splitter?
1 composite video PAL/NTCS IN, 3 composite video PAL/NTCS OUT, to 3 different Analog monitors?
If the answer is No, can you please suggest me how can I split 1 video IN to 3 video OUT?
My JPEG saga continue...
I am using a BF561 single core to compress a 640x480 YUV 4:2:2 image into JPEG format, employing the ADI JPEG Library tools. I am getting very poor performance compared with the reference results from the Spec Sheet. The Spec…
Hello Dave,
I am facing problems with replies to your answer, so I am oppening a new dicussion with the same title.
Please clarify your answer regarding STANAG support:
2) As I understand it, this is the same as RS-343A/EIA-343A and none of our parts…
Hello,
I installed 2x LTC6811-2 and then 1x LTC6804-2 on the same board and I don't have any voltage reference output at anytime. The functional diagram in the datasheets shows that VREF1 should be always present as it's generated from V+. VREF2 is not…
I am using the ADM1176-2 (latching) part on a new PCB design. I am wondering if setting the SWOFF bit over I2C can reset the latch state the same as toggling the ON pin? The datasheet isn't entirely clear on this aspect--on Page 16 Table 11, it states…
Iam interested in implementing a MIMO 2*2 scenario where i will use 2 fpgas (1 as the transmitter and 1 as the receiver) where each one will be connected with one AD-FMCOMMS3-EBZ. So the setup will be : FPGA_1 + AD-FMCOMMS3-EBZ_1 =Base stati…
Can the ADV7403 output YUV 4:2:2 rather than YCbCr 4:2:2?
Thanks.
Chris