• RE: Considering AD7606B but need more PGA ranges (down to +-20mV)

    Hello Liuis,

    I'm getting to know the ADA4254 - this is a nice device that solves a lot of problems for me. I had it hooked up to the AD7768 eval today and got some very good results.

    However, my challenge will be synchronising the AD7768 to sample…

  • LTC2324-16 REFOUT as an output for resistor division

    I have a question regarding the Linear LTC2324-16:

    I'm using the external reference through REF pin (general for all ADC). Can I use REFOUTx as an output for resistor division for input VOCM pin ADA4254? ((REFOUT (that is my external reference) Voltage…

  • RE: AD8422增益控制

    输入不能浮空,浮空会导致很多的不确定性,比如有一个漏电流流入你的AD8422,而AD8422的输入阻抗又很高,可能会导致产生一个不确定的电平。如果你想确定你的增益正常,需要将输入接地。VDD断开后,你的运放不工作,当然信号为0.

    你可以看看我们的可编程增益仪表放大器PGIA,比如ADA4254和LTC6373

  • Ad7768-1 external component selection

    Just to help clarify things for me, I’m designing a circuit for a general purpose daq application (goal being lowest achievable noise from ~1ksps to ~64ksps) with the ad7768-1, ada4254, and TBD external reference. Looking at the datasheet for the amplifier…

  • RE: Ask a question about SAR ADC ANALOG INPUT ARCHITECTURES

    Hello,

    Hopefully the sketch below clears this up. Basically the scenario described is if you have some sensor, etc. that has a large common-mode output voltage. In the figure provided, this is represented by VCM.

    For many ADCs, connecting such a sensor…

  • 3-4月ADI新品主打,快来康康有没有适合你的设计~

    携一缕浅夏的芬芳,凝一脂冰清玉洁的清梦

    各位小伙伴们,迷人的仲夏五月来啦~

    在这个似水的季节里,悠然翻阅学习岂不美哉?

    今天斑竹给大家带来 ADI 3 - 4月的新品合集,想要了解学习的筒子可千万不能错过哦~

    MxFETM四通道 16 位 12GSPS RFDAC 和双通道 12 位 6GSPS RFADC AD9082

    发射信号前端 (MxFE®) 是一款高度集成的器件,具有 16 位、12 GSPS 最大采样率射频 (RF) 数模转换器 (DAC) 内核和 12 位、6 GSPS 采样率…

  • 在新年到来之际,送你一组钻石级硬度的精选硬核产品吧~

    转眼间,2020年就要结束了,今年你都做了些什么呢?

    对于ADI,我们可是推出了不少硬核产品哦~

    今天,斑竹就给大家晒晒ADI这些杠杠滴成果!

    -------------------------------------------------------------------------

    软件可配置的四通道输入/输出 AD74413R

    AD74413R是一款软件可配置的四通道输入/输出解决方案,适用于楼宇和过程控制应用。AD74413R包含用于模拟输出、模拟输入、数字输入、电阻温度检测器(RTD…

  • ADI 全新中文资料(2020 年 2 月)

  • 2020年 ADI 20款硬核新品,为你献上电路设计的不二之选

    你最关注的领域是什么?ADC/DAC?Power?RF?.....

    你知道ADI在这些领域都推出了怎样的硬核新品吗?

    回首2020年,虽然被疫情干扰,不过咱ADI依旧没有停止推出新产品的脚步,今天斑竹就为大家盘点一下今年的“新秀”吧~

    四通道、软件可配置输入/输出 AD74412R/13R

    AD74412R 是一款适用于楼宇和过程控制应用的四通道软件可配置输入/输出解决方案。AD74412R 包含用于模拟输出、模拟输入、数字输入和电阻温度检测器 (RTD) 测量的功能,这些功能集成在一个单芯片解决方案中…

  • AD7134: FAQs

    Q1. What anti-alias filter is required for AD7134?

    The architecture of AD7134 offers excellent attenuation of out of band high frequencies providing 102 dB inherent Alias rejection which caters for most of the application requirements.

    Along with the…