ADA4177-1是否可以单电源供电,只用+5V供电可以么?谢谢!
We have purchased ADA4177 IC from Element14 , QTY 1000 for company requirement.
But frequent failure observed for same IC in our PCB where we are using IC ADA4177 (at location U3 only, though U11 is also same IC). We have done failure part analysis at…
Hi
Can I use the opamp ADA4177-2 in single supply operation?
It is specified for +/- 15V.
Can I apply 28V dc to positive supply rail V+ and ground V-
I plan to bias the input to the chip at 14V dc.
Thanks
Sreelakshmi R
This is a simple circuit intended to replace any dual op-amp in dip 8 pkg.
Short question is , is there any tendency on this part (ADA4177-4) to self oscillate? Probably not but wanted to ask.
I have a new layout that is self oscillating…
Recently, I received sample IC ADA4177-4ARZ from Analog devices. When I just given +15V and -15V supply at pin 4 and 11 respectively, without giving any input and also no output connection, the IC started heating too much. My project requires +15 to -15V…
Hi
Can we evaluate OVP function in LTSPICE?
Because below result don't coincide on Datasheets' .
Best regards
Thank you very much.
请问:
ADA4177电路性能优秀,是否用DC/DC 电源(纹波30~100mV)会大大降低性能,是否需要用LDO电源供电呢,ADI有这个OP的供电方案不?
谢谢!
There are many considerations when driving an ADC. A primary consideration is the noise and linearity of the amplifier driving the ADC. The effective resolution of an ADC is affected by its total harmonic distortion and noise (called “SINAD” in ADCs…
请问:
信号特性:0~3V 单端电压信号
输入阻抗5K
带宽10K,低速(10mV/ms)
4路
在滤波后送给MCU的ADC采样引脚。
看到 ADA4177-4具有优越的性能,而且保护功能也和独到,是否可以使用它来实现上述信号的滤波呢?
谢谢!