Q
What major improvements does this family (ADA4077-2) offer to applications?
A
Almost all specs are improved over the previous generations. The biggestimprovement offered to various applications by ADA4077 is the wider bandwidth
to process…
Hi
datasheet on page 13 states that the ADV7612 supports 36-bit 4:4:4 YCrCb, but the table 5 and 6 do not list this mode. Is it supported, how can it be activated?
best regards
Dani
I have a question. What is the content of Section AV for YCbCr 4:4:4 24 bit interface?
Page 13 of DS describes the PIXEL INPUT/OUTPUT FORMATTING The output section of the ADV7612 is highly flexible. The pixel output bus can support up to 36-bit 4:4:4 YCrCb or 36-bit 4:4:4 RGB. The pixel data supports both single and double data rates modes1…
Hello,
I wanted to ask for clarification on the VS and HS signals with the ADV7619 in pass through mode. i read the thread on this previously https://ez.analog.com/message/156902#156902 and it does say that the CP will be bypassed and the syncs remain…
Could you please provide the IIC configuration script for ADV7511 HDMI
I am working on the ADV7511 chip, which is the HDMI codec in VC707 EVB from
FPGA company Xilinx.
I want to configured the ADV7511 working in 1080P, 4:4:4 RGB input (each
component…