Hi,
I got a notice from Digi-Key that the ADA4075 is marked end of life. Checking the product Page there is no such info.
I just finished a design using this OpAmp. Is it still recommended for new designs?
Hi,
I got a notice from Digi-Key that the ADA4075 is marked end of life. Checking the product Page there is no such info.
I just finished a design using this OpAmp. Is it still recommended for new designs?
For a low noise dual opamp I selected the ADA4075-2 based on the datasheet "typical" spec of 60 nVpp noise at f = 0.1 Hz to 10 Hz. There is no worst-case spec on the data sheet.
The analog.com site features an article by James Bryant which makes…
Hello Technical Support,
I seek to understand the input parameters related to precision (namely: Vos, & Ib) as a function of common-mode input voltage, for the ADA4075-2.
The datasheet I have is ver C, dated 11/13.
On datasheet page 3 the table states…
Hello,
I have got an amplifier which is working pretty well with ADA4004-2, OP284 & AD8599 Low Noise OA's.
Please see schematic attached, it has two +/-5V supply lines.
ADA4075-2 is 3-4 times cheaper, so it is more attractive on that reason
…
I want to use ADA4075 for a differential input that could have a maximum of 10V differential voltage.
In the datasheet, I see the absolute maximum rating for Differential Input Voltage is ±1.2 V
What does this mean? The Inputs should have a difference…
Hi,
I would like to setup the SDR Pluto to operate in 2 Tx and 2 Rx mode.
I have followed the steps in the following video : https://www.youtube.com/watch?v=ph0Kv4SgSuI
However, I am unsure how to setup and control the 2nd transmitter or receiver.
…Hi,
With a bit late, thanks for this suggestion.
By applying -0.2V to R3, this circuits can convert 0 to 0.4V to a balanced -0.2 to 0.2V .
It has been checked on the eval board.
I am trying to configure ADV7611 to output 1280x1024 video in 16-bit SDR ITU-R BT.656 4:2:2 Mode 0.
In free-run mode with blue background I get "0xFF00, 0x0000, 0xFF00, 0x0000..." pixel data, but it is 1280 LLC-period wide DE window between HSyncs…
Hi ADI support team. I use LTM4671 in my new design. The datasheet of this device is here: www.analog.com/.../LTM4671.pdf I wonder whether there are two mistakes in the figure2 of datasheet? For 2+2 parallel application, I think PHMODE0 must connect to…