Worse case power dissipation (Pd) & Thermal resistance θjc (Junction to Case) required
Worse case power dissipation (Pd) & Thermal resistance θjc (Junction to Case) required
Hello,
The some datasheet that it have describe the input resistance, like ADA4051, but the others datasheet didn't describe the input resistance, like AD8539 and AD8500
How to know input resistance? especially no describe the input resistance???
…Hi,
I am trying to use the ada4051 in a differential amplifier configuration. Attached below is a schematic of the circuit with the components being used, ltspice schematic , and a graph comparing outputs. In image one, the high and low inputs are from…
Hi,
I am goning to distribute a common 40 MHz clock to 2 DDSs and 2 ADCs. Will AD9577 work for this purpose? If not, do you have any suggestion?
The ADC needs 5 V CLK and the DDS needs 1.8 V CLK.
My JPEG saga continue...
I am using a BF561 single core to compress a 640x480 YUV 4:2:2 image into JPEG format, employing the ADI JPEG Library tools. I am getting very poor performance compared with the reference results from the Spec Sheet. The Spec…
Hello Dave,
I am facing problems with replies to your answer, so I am oppening a new dicussion with the same title.
Please clarify your answer regarding STANAG support:
2) As I understand it, this is the same as RS-343A/EIA-343A and none of our parts…
Hello,
I installed 2x LTC6811-2 and then 1x LTC6804-2 on the same board and I don't have any voltage reference output at anytime. The functional diagram in the datasheets shows that VREF1 should be always present as it's generated from V+. VREF2 is not…
Hello,
Iam interested in implementing a MIMO 2*2 scenario where i will use 2 fpgas (1 as the transmitter and 1 as the receiver) where each one will be connected with one AD-FMCOMMS3-EBZ.
So the setup will be :
FPGA_1 + AD-FMCOMMS3-EBZ_1 =Base stati…
Can the ADV7403 output YUV 4:2:2 rather than YCbCr 4:2:2?
Thanks.
Chris
Hi,
I have the EVAL-ADV7612-7511p video evaluation board .I'm using 7612 to receive HDMI inputs from camera(720p @60) , and then feed to 7511 to output the video to the screen.
camera -> 7612 --> 7511 --> screen
When adv7612 output 4:4:4 8bit ycrcb…