• ADA4051-2ARMZ-R7

    Worse case power dissipation (Pd) & Thermal resistance θjc (Junction to Case) required

  • AD8500/AD8539/ADA4051 Input resistance

    Hello,

    The some datasheet that it have describe the input resistance, like ADA4051, but the others datasheet didn't describe the input resistance, like AD8539 and AD8500

    How to know input resistance?    especially no describe the input resistance???

  • ADA4051-1AKSZ/2ARMZ Differential amplifier configuration

    Hi, 

    I am trying to use the ada4051 in a differential amplifier configuration. Attached below is a schematic of the circuit with the components being used, ltspice schematic , and a graph comparing outputs. In image one, the high and low inputs are from…

  • wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    The LT8708EUHG-1#PBF specification shows that the LT8708-1 always operates as a slave to the master LT8708, Mainly used in parallel with LT8708, At present, our customer wants to use LT8708-1 (LT8708EUHG-1#PBF) separately without parallel connection.…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh

  • Can LT8708EUHG-1 be used as a standalone DC-DC?Can LT8708EUHG-1 be used as a standalone DC-DC?

    Can LT8708EUHG-1 be used as a standalone DC-DC? Can LT8708EUHG-1 be used alone? Can LT8708EUHG-1 work alone?