• ADA4004 Distortion

    Hi, 

    I'm trying to incorporate ADA4004 in my next audio design as a low power replacement of OPA1612. Is there any data on its THD?

    Thanks, 

    Bo Gao

  • ADA4004 Input Impedance

    Greeting.

    I am selecting an amplifier as the Pre-Amp of a VGA and I comes to ADA4004

    The datasheet provides detail performance data but not the Input Impedance (Res and Cap)

    Where can I access those information?

  • ADA4004: Maximum Differential Input Voltage

    We are using ADA4004 OP-Amp in an application with high differential input
    voltage. (0...10V). It is supplied with +-15V. Do the inputs of this Opamp draw
    higher input currents, with this differential input voltages?
    Will there any other…
  • ADA4004 - differential to single ended conversion

    Hello,

    I would like use the proposal from:

    https://www.analog.com/media/en/analog-dialogue/raqs/raq-issue-145.pdf

    First I did the simulation in LTSpice using ADA4004-2 (selected for that solution)

    I expect the audio frequency spectrum will be stable…

  • Problem with ADA4004-4/ADG1436/AD7628

    Dear All:

    Recently I had a full board using, among others, the chips named above. As I got ADA4004 or ADG1436 burnt without any explanation, I did a prototype board using only the above chips to try to discover the problem and still have the same problem…

  • Is the ADA4004-2 unity gain stable as an inverting amplifier?

    Hello,

    From experience, a datasheet for an op amp will say whether or not the op amp is unity gain stable.  I cannot find such a statement for the ADA4004-2.  Does anyone know if this particular op amp is unity gain stable?  I'm especially curious if this…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • LTM4644-1 LT POWER CAD 3+1 MODEL,

    CAN YOU POINT ME TO THE POWER CAD MODEL FOR 3+1, I ALREADY HAVE THE 2+2 AND 4.

    I WANT TO MAKE SURE I GET THE COMPENSATION VALUES CORRECT BEFORE BUILD.