• Can ADA4000-4 work on +-18V power supply?

    Hello,

    I am searching one kind of opamp to work on +-18V. ADA4000-4  may be the choice as the datasheet said that "±4 V to ±18 V operation". However, I also found in the datasheet that the maximum supply voltage is "±18 V".

    So my…

  • ADA4000 stability issue

    I tried replacing a TL082 which was working fine in the attached circuit with ADA4000.

    I am very unhappy with the stability fo ADA4000. The input is from an DAC (100KHz) and the output is at output pin of Opamp.

    What could be a direct replacement for…

  • RE: ADA4000 comparator

    Hi David,

    I just read your answer, I will try to check on devices what happens taking into account your question.

    I also have additional clues for this issue. ADA4000 datasheet precises that without voltage supplies (power voltages), input current…

  • RE: OP4177 opamp is not working as voltage limiter.

    FormerMember
    FormerMember

    Ruchi,

    I think you might be stuck.  The precsion bipolar op amps usually have diodes between the inputs to protect the diff pair so you don't zener the EB junction.  You might look at some of the JFET op amps, such as the ADA4000-4 or the AD8513, but…

  • RE: AD711 replacement solution

    Hi,

    Recommended alternative parts for AD711 from the product page in this link are:

    ADA4000-1

    ADA4610-1

  • RE: How to protect ADA4000 inputs from momentary over-voltage?

    Hi,

    You can refer to this link regarding maximum safe input overload condition of ADA4000.

  • ADA4000-1输出电流最大能到多少

    ADA4000-1输出电流驱动能力最大能到多少

  • RE: anveshan 2015080: AD8606 is getting heated up

    Hi Koushik,

    How is your circuit coming along so far? I think it would be easy for you to just maintain your original schematic and replace the AD8606 parts with any one of these: ADA4610-2 (Dual), ADA4610-4(Quad) and ADA4000-4(Quad). These parts really…

  • RE: ADG901  Switch condition under power off (Vcc=0V)

    Further to this.  I have attached an application note about the ADG4612 part.  This app note also shows what happens to our regular analog switches if you apply a signal with no supply voltage present (see Figure 2).

    Regards,

    Eric.