• RE: ADA2200 usage

    Hello Syam,

    The ADA2200 is being discontinued, so you may want to look for an alternative device if you are planning on building this circuit in the future.  This article details a couple of alternatives to the ADA2200.

    The input to the ADA2200 does not…

  • ADA2200 fclkin limit

    Its seems that from the datasheet that the fclkin is limited to 1MHz when CLKIN DIV[2:0] = 1. This seems to indicate that the center frequency of the fm is limited to (1e6/64). I have tested the ADA2200 at up to fclkin of 3.2MHz and a 3.2MHz/64 carrier…

  • Syncing two ADA2200s

    I am using two ADA2200-EVAL boards to work as a lock in amplifier. We need to have both the in quadrature and out of quadrature measurements at the same time in order to get accurate results. Both boards are receiving a clock in signal from the same source…

  • ADA2200 suitable for my application?

    Hi, for a project I have a signal that is already modulated with a carrier frequency of about 15kHz (can be altered if needed, preferably higher). For demodulation of this signal I was thinking about using the ADA2200. After reading a bit through the…

  • RE: ADA2200 simulation

    Hi, 

    Apologies for missing this item. I am not sure if it still relevant to you that this question will be answered, However, we are clearing up some open items in our community and ensure that any other query is located on its proper community as others…

  • ADA2200 EVALZ Help

    Hello,

    I have been working on replacing a test setup at my company that utilizes a Lock In Amplifier, and I am running into some issues due to a lack of understanding on my part.

    To preface this, I will say that the test equipment is most likely from…

  • RE: ADA2200 sine wave

    Hi, 

    Apologies for missing this item. I am not sure if it still relevant to you that this question will be answered, However, we are clearing up some open items in our community and ensure that any other query is located on its proper community as others…

  • ADA2200 Data Sheet

    Specifications on pg 3 of the ADA2200 Data Sheet, Rev. 0, constrain minimum CLKIN frequency to be from 10 KHz to 2.56 MHz.

    Within the FAQ and Q&A, there are several examples of statements that contradict the specifications, indicating CLKIN|min = 1 KHz…

  • ADA2200 怎么从EEPROM引导

    ADA2200 怎么从EEPROM引导

  • ADA2200 解调器 的LTSPICE 中模型无法使用

    我在官网下载了ADA2200 的PSPICE 模型并加载到LTSPICE 仿真软件中,在执行仿真命令时提示 undefined subcircuit ::。不知道是否哪里出错了。。。