• RE: AD9985

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD9985找替代型号芯片

    之前产品一直采用的AD9985进行VGA采集解码,现在项目需求变更,VGA分辨率更改为1400*1050,按照AD9985手册(最大支持分辨率1280*1024)无法满足项目需求,而官网推荐替代器件ADV7842温度是0-70,现在想找一款替代AD9985(满足1440*1050/60hz采集)的器件(能PIN TO PIN替代AD9985最好),要求工业级(-40℃-+85),最好有推荐的硬件设计资料,希望技术给予支持,谢谢!!!

  • RE: AD9985 output operation

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Can the 9984A convert an RGB signal into (3) 8-bit channels, or can it only output in 10-bit?

    Thanks so much for responding.

    I have an analog R-G-B input (stream) that is already 8-bit per stream. I need to convert that analog stream into a digital one (3 channels @ 8-bit each) that can be understood by an HDMI transmitter such as the ADV7513…

  • AD9985A Design Support Files

    The AD9985A is a triple ADC for processing RGB and Video graphics in automotive and industrial applications.  Relavent deisign support files are attached here.

  • RE: Power-on-reset of AD9985A (ADW10000BSTZRL-110).

    Hi Tamu,

    AD9985A product status is "Not Recommended for New Designs". I think AD9985 product status should be the same. I will confirm this.

    Is this a new product or an existing product?

    -Matt

  • RE: AD9985A

    Hello,

    First of all the AD9985 does not have a way to adjust the VS pulse width based on line count like the HS pulse width based on pixel clock.

    Second of all I'm a bit confused.  If we look at VESA standard 848 x 480 @ 60 (which is close to your…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…