• RE: What kind of level standard is it for AD9963 diff CLKP/N?

    information in the datasheet : DRIVING THE CLOCK INPUT

  • AD9963 datasheet errata?

    I'm working with a board with the AD9963. In debugging our designs, I've observed some behaviors different from those described in the "Rev. 0" datasheet.

    I believe AD9963's interpretation of the following register bits is inverted…

  • AD9963. Problems.

    I am using the AD9963 chip now and I have found a few mistakes in the datasheet. I have attached the file below (datasheet_AD9963.pdf).

    I have not found any information about using FIFO Alignment register 0x33. How can I set the FIFO read and write pointers…

  • AD9963 clock doubler

    Hi all,

    In the datasheet @ AD9963, about the clock doubler is following.
    "CONFIGURING THE CLOCK DOUBLERS
    The receive and transmit data paths each have a clock doubler used for clocking data through the device.
    These clock doublers are only used in single…

  • AD9963 clock doubler

    Hi all,

    In the datasheet @ AD9963, about the clock doubler is following.
    "CONFIGURING THE CLOCK DOUBLERS
    The receive and transmit data paths each have a clock doubler used for clocking data through the device.
    These clock doublers are only used in single…

  • AD9963 Quick Start Guide

    Hi all,

    AD9963 Quick Start Guide and other files are not available following link.

    Please provide the following files or new links.

    AD996x Evaluation Board

    http://wiki.analog.com/resources/eval/dpg/eval-ad996x

    Quick Start Guide
    IBIS Models: AD9963,…

  • Sync two AD9963

    Hi, in my application, I want to use 2pcs of AD9963 on one board to get a Quad channel ADC inputs + Quad Channel DAC outputs, is it possible to sync these two AD9963 by bypassing the DLLs? Drive two 9963's CLK with a CLK distribution chip instead, will…

  • AD9963 DAC configuration

    Hi,

    I need to transmit a 8MHz GMSK signal from AD9963 DAC. Until now we have been using it to transmit 2MHz GMSK and there were no problems. However when we started to transmit higher symbol rate I noticed large IQ imbalance at the DAC output.

    I used…

  • AD9963 can NOT run

    我将AD9963评估板和DPGIOZ连接,且都用USB连接到了PC,并按quick start文档配置了电源和时钟,但是PC端的SPI软件和DPGDownload软件仍然无法加载AD9963的数据模板,也无法向芯片加载数据,求各位大神解惑!

    The AD9963 linked to DPGIOZ, and both of them linked to PC by USB.

    The power and clock configured according to the quick start document…

  • AD9963 ADC Latency

    Hi,

     

    I appreciate if some one can tell me the delay from the sampling of receive signal to the time presented to the TRXD.  It is unavailable in the datasheet.

     

    Thanks

    Henry