Hello,
I have an AD9961 connected to ADSP BF561. I want to read the I and Q samples available on the TRXD[11:0] pins. How can I read this data directly? I went through various internal registers of MXFE but like the various control registers, this data…
We can offer to replace the AD9861 eval board that is no longer reccomended for new designs with the AD9961 eval board. We will not be able to support the AD9861 eval board questions.
My apologies I answered you based on the AD9961 and AD9963. The AD9761 and AD9763 were introduced in 1999. The AD9763 and AD9761 are not recommended for new designs. You can look for alternatives in the selection table for high speed DACs on www.analog…
Hi all,
AD9963 Quick Start Guide and other files are not available following link.
Please provide the following files or new links.
AD996x Evaluation Board
http://wiki.analog.com/resources/eval/dpg/eval-ad996x
Quick Start GuideIBIS Models: AD9963,…
Hi Del- san,
Thank you for your reply!Again, is the correct understanding that the clock doubler and the interpolation or decimation filters cannot be used at the same time?
The customer asked us an additional question,1.What is the DAC output level …
You didn't mention the receive chain... there are a couple of alternatives. The AD9957, which is a DDS modulator, can create a modulated IF that you can mix into this range so you would only need a mixer and PLL/VCO. I thnk it's fast enough for 1.2 MBPS…
Hi Rain -
You should be seeing 1.4V DC on the RXCML pin if the RXCML pin output buffer is enabled.
Are you following this programming sequence from page 21 of teh data sheet?
SUB SERIAL INTERFACE COMMUNICATIONS
The AD9963/AD9961 have two registers…