FAQ
Hi. I use SPI communication to control the AD9958. Is it possible to read the value in the I/O port buffer before transferring the data to the register?
I hope to hear your response. Thank you.
【Detailed Block Diagram】
【Product】
AD9958 / PCBZ
On the AD9958, what is the minimum time allowed after MRST goes low before SPI communications can begin and function as normal? I think I am not waiting long enough on my part and it is affecting the performance. Right now there is a 10ns gap between…
Hello everyone,I am a PhD student and I am looking for a solution to replace a DDS-based RF signal generator (AD9958) on a homemade evaluation board with a similar commercial one. Specifically, I need a generator that creates an RF signal characterised…
I have a question regarding fast recovery power-down mode and the PWR_DWN_CTL bit for the AD9958
When placing this device in power down mode using the external bit, am I still able to update the internal registers via SPI bus? And use IO Update to store…
I have a question regarding the behavior of IO_UPDATE with the timing of an SPI transaction.
Here's the scenario:
Let's say I program in a linear sweep to the DDS, then pulse the update. Immediately after, I program in another linear sweep, but do…
I have an AD9958 installed on a custom PCB, and I am running into a problem with communication with the part. Registers 0, 1, and 2 can be written to, read from, and changed, and I can see their effects on the part from a scope (can change SYNC_CLK speed…
Hi all,
Our customer will design the custom board with AD9958.
They have the question about the Loop_Filer, 27pin.
@ the datasheet rev.c,
27 pin description ;
Connects to the external zero compensation network of the PLL loop filter.
Typically, the network…
I am using the AD9958 to conduct a linear sweep, using P2 and P3 to toggle the sweep up and sweep down of said sweep.
However, I would also like to use the phase modulation capabilities of this part to swap the phase 180 degrees at the peaks of my sweeps…