• AD9889B: does the AD9889B support the format 1080i50

    I wanted to know if AD9889B supports the Video Format 1080i-50?

     

    Yes, the AD9889B does support 1080i50. As long as a format is within the
    maximum clock range (150MHz), then it can be supported. There is nothing that
    is specific to the support…

  • AD9889B/AD9389B Design Support Files

    Attached and linked are several files supporting the development of systems using the AD9889B (HDCP keys stored externally in EEPROM) or the AD9389B (HDCP keys stored internally).

    We recommend if you download and use these documents that you subscribe…

  • RE: ad9889b color problem

    This question has been closed by the EZ team and is assumed answered.
  • AD9889B hdmi Interlaced output question

    The HDMI analyzer shows that the format of ad9889b hdmi output is progressive in 1080i50/59.94/60 and 576i/480i.

    it shows that the vtotal of 1080i50/60 is 562, the vtotal of 576i50 is 313, the vtotal of 480i60 is 262,  

    Hdmi output timing is reference cea…

  • RE: AD9889B as DVI transmitter

    This question has been closed by the EZ team and is assumed answered.
  • RE: I2S audio on AD9889b

    This question has been closed by the EZ team and is assumed answered.
  • RE: AD9889B setup

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9889B usage

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9889B: No Video out and no TMDS out clocks

    This question has been closed by the EZ team and is assumed answered.