• Looking for alternate Part: AD9888

    Hi Analog team,

    I am redesign one of KVM-Over-IP product, where AD9888 was used.

    Now AD9888 is not recommend to use in new design. So I am looking for alternate part number which supports VGA analog input. Supported maximum resolution 1600x1200@60Hz is…

  • RE: AD9888 scripts

    Hi,

       ADV7604 can meet your requirement.

      Can you please check the design support file and let us know if any dependency.

    Thanks,

    Poornima

  • RE: A issue about AD9888 operation

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9888 vertical noise - left/right pixel alternating

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD9888: What time is required to achieve a stable video output once the power down bit is de-asserted?

    How much time does the AD9888 need to settle on the video signal and deliver a
    stable video data output
    after the converter is taken out of power-down mode.

     

    We estimate that it takes about 20mS to achieve a stable image out once the…
  • AD9888 HDMI compatibiltiy issures with modern pro camcorders

    I am looking for an expert on the AD9888 HDMI Input Chip. So I am hoping somebody can give me an idea on a problem we have with the AD9888. 4 years ago we designed a few of this chip into our "presentation recorder" which is a special kind of lecture…

  • AD9888 power related issue

    Hi,

    Power relevant issue occurred on my customer's product on which AD9888 is used.

    The detail is as follows.

    The end-user powered up the product and keep on for more than 20,000 hours.

    After that, they turned off the product for the periodic…

  • RE: AD9826 power down

    Hi,

      Please refer below comments,

          How much time does the AD9888 need to settle on the video signal and deliver a stable video data output
    after the converter is taken out of power-down mode ?

              Estimated that it takes about 20mS to achieve a stable…

  • RE: support VGA?

    Hi,

    ADI will shutdown AD9888? AD9888 has three types:140M,170M,205M, So AD9888 can support 1600*1200@60 and 1080p60. I don't understand what's the meaning is AD9888 is no longer supported.

    Thank you

    Tom