• DDS Features Chart

    Frequently we're asked for help selecting a DDS with frequency sweeping capability, phase hopping, amplitude control etc. but until now the only way to answer that question was to go based on memory or to look at the datasheets for several DDS parts.…

  • DDS: Testing, and Application Signal Chain Building using AD9834

    Hi! Kevin, Thanks alot firstly, for helping on my queries. It helps.

    As informed earlier, I'm possessing two signal generators 33250A (Agilents).

    However, I want STEPWISE verrification of VPHS o/p swing from 30mV to 1.8 V using DDS (ad9834) as one…

  • RE: 有没有运用AD9851的中文资料?

    刚在网上搜到的,请楼主看看.

  • RE: AD9858的DDS无输出

    如下附件有DDS 的常见问题,可以检查一下,是否有类似的问题

  • 附件是DDS的常见问题解答。内容包括ADI的DDS产品,DDS的原理以及DDS常见问题。

    希望可以帮助大家

  • ADI处理器实用经典著作—《高速设计技术》中文电子版

    本书内容包括三大部分:


    1 部分从运算放大器的基本概念和理论出发,重点介绍了运算放大器的原理与设计,以及在各种电子系统中的应用,包括视频应用、RF/IF 子系统(乘法器、调制器和混频器)等;

    2 部分主要介绍了高速采样和高速ADC 及其应用、高速DAC 及其应用、以及DDS 系统与接收机子系统等;

    3 部分介绍了有关高速硬件设计技术,如仿真、建模、原型、布局、去藕与接地,以及EMI RFI设计考虑等。

    书中内容既有完整的理论分析,又有具体的实际应用电路,还包括许多应用技巧。特别适合电子电路与系统设计工程师…