Hi,
I have a AD9785 Evaluation Board. I connect USBto PC and run ACE software , it recognize board but in state it write State = Unkown and i can't reset or program it;
Hi,
I have a AD9785 Evaluation Board. I connect USBto PC and run ACE software , it recognize board but in state it write State = Unkown and i can't reset or program it;
Whenever I am probing the output on L1,L2,L3,L4 connected to the pins OUT1_P,OUT1_N,OUT2_P,OUT2_N it always shows 3.3V before and after programming. I have cross checked every connection as per the reference schematic and nothing was changed significantly…
关于AD9785评估板:
(1)EVAL-DPG 数据模式发生器(DPG)高速DAC评估平台
(2)DPG2 - Data Pattern Generator (DPG) High-Speed DAC Evaluation Platform
…您好!我买的AD9785-DPG2-EBZ和AD9627-150EBZ 这两款评估板是否可以通过背板连接线连在一起实验。即将模拟信号经过我的这个AD评估板,然后直接经过DA评估板,转换为原来的模拟信号?这个方案可行吗?如果可以的话,应该怎么连接这两个板子的连接器件将这两个板子连接在一起了?如果不可以的话,原因是什么了?
另外一个问题:对于AD9627这款评估板(绿色的),背板连接器的输出信号是哪些引脚了?同样,对于AD9785这款评估板(蓝色的),背板连接器哪些引脚是输入信号?也就是这两块板子的背板连接器该如何连接起来了…
Hi
The purpose is to apply DAC(AD9785) differential output signals to the I/Q mixer (HMC1056LP1BE), and in this design, balun should be used to convert the differential signal to single-ended and then apply to the mixer (HMC1056LP1BE).
1)We want use hmc1056…
HELLO
I have a evaluation board EVAL-AD9785 for testing in 2 GHz with ADL5375 modulator and IQ modulator HMC1056LP1BE and EVAL-HMC765LP6CE for testing in 8 GHz.
when I use EVAL-AD9785 and connect output to the spectrum in 2.4GHz and we can see spectrum and…
Hello Jaime,
Thank you for your interest in AD9785/7/8.
If you connect the evaluation board directly to the computer and provide a 5V 1A supply to P4/P5, you would be able to control the SPI of the DAC using ACE. However, since the data inputs and DCO…