• RE: AD9760 output constant

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Setup and hold timing in AD9670

    Hi,

    I am trying to interface the AD9760 with a FPGA, I need to constrain timing input.

    In datasheet, it talks about DCO to Data (Tsample/28 +/- 300ps).. 

    In worst case, I guessed that setup and hold time are Tdco/4 - 300ps. But it is not clear for us…

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    合肥  经济技术开发区  电源 关注   AD9760

  • RE: AD9764 output

    Hi

    In the AN-420 application note about using the AD9764-EB Evaluation Board it is suggested to use C12,C13=22 pF and R20,R38=50 Ohm (as can be seen from the attached image).

    It is also said that :

    " OUTPUT CONFIGURATIONS

    Resistive Load

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • ADI处理器实用经典著作—《高速设计技术》中文电子版

    本书内容包括三大部分:


    1 部分从运算放大器的基本概念和理论出发,重点介绍了运算放大器的原理与设计,以及在各种电子系统中的应用,包括视频应用、RF/IF 子系统(乘法器、调制器和混频器)等;

    2 部分主要介绍了高速采样和高速ADC 及其应用、高速DAC 及其应用、以及DDS 系统与接收机子系统等;

    3 部分介绍了有关高速硬件设计技术,如仿真、建模、原型、布局、去藕与接地,以及EMI RFI设计考虑等。

    书中内容既有完整的理论分析,又有具体的实际应用电路,还包括许多应用技巧。特别适合电子电路与系统设计工程师…