• AD9747 single port mode

    AD9747 in single port mode ,how i handle the IQSEL pin?

  • AD9747

    I have some question about AD9747.

    Can you tell me the answers of these question.

     

    Q1.
    In the case of using DAC1 only, should I connect IQSEL(pin29) to DVDD ?
    Or,
    Should I connect IQSEL(pin29) to FPGA or other ?

     

    Q2.
    Can I apply the Op Amp-Coupled Output…

  • AD9747

    Sir,

    I have AD9747 evaluation board, AD-DAC-FMC-ADP board and XILINX KINTEX KC705 board.

    i want to operate it, but couldn't find the required software. need your assistance. 

    Thanks in advance

  • About AD9747

    When we use the AD974, we find the data input to P2D port have 9-10 period delay with the data input to IOUT2P and IOUT2N. We want to know the reason why it happend. In the figure,  Channel 1(yellow) is the data input curve, Channel 2(red) is the Voltage…

  • About AD9747

    When we use the AD974, we find the data input to P2D port have 9-10 period delay with the data input to IOUT2P and IOUT2N. We want to know the reason why it happend. In the figure,  Channel 1(yellow) is the data input curve, Channel 2(red) is the Voltage…

  • AD9747: Thermal Information

    For carrying out the analysis the following part specifications are necessary:

    1)Power Dissipation (W)
    2)Junction Temperature (TJ)
    3)Case Temperature (Tc)
    4)Junction to ambient thermal resistance (θJA)
    5)Junction to case thermal…
  • AD9747 doesn't work

    Hi,

    I'm working on the bring up of a new custom PCB including the AD9747.

    In one of the very first trials, I could get it to run a simple ramp on its output, but with no other design in my FPGA it will provide any output.

    I've already tried writing…

  • Ad9747 DPG2 EVB

    I am using AD9747 DPG2 EBZ and xilinx kintex-7 and I downloanded DAC Software Suite but the software incomplete, DPGDownloader window are Vector Generation Pull-Down Menu, Vector Palette only but Hardware Config Panel and EVB Config not found, how can…

  • AD9747 Clock Driver

    Hi every one,

    I want to drive LVDS clock for AD9747 from Spartan3E. What I read from AD9747 datasheet was that the minimum LVDS pair is 400mV but from xilinx datasheet I found that typically it is around 350mV. What can I do? Should I just connect the…

  • AD9747 evaluation Board

    my AD9747 Evaluation Board cannot run.  Which PIC18F4550 clock does not work.As a result, the USB interface cannot work, so the entire development board cannot be set