AD9746输出时有信号的谐波是什么问题啊,比如DA输出30MHz,DA时钟频率120MHz,DA的输出就会有60MHz,90MHz的信号。请问这是什么问题,怎么解决,谢谢。
AD9746输出时有信号的谐波是什么问题啊,比如DA输出30MHz,DA时钟频率120MHz,DA的输出就会有60MHz,90MHz的信号。请问这是什么问题,怎么解决,谢谢。
Dear Sirs,
We are using AD high speed DAC AD9746 on one of our board.
The DAC is configured in single port mode with data coming from a FPGA. We are
seeing some issues with clocking data into the DAC. From the datasheet it was
not clear when the data…
大家好,
我最近在调试一块发射通道时遇到的问题
使用AD9746配合ADRF6755做正交调制,输出频谱中存在大量DAC时钟的偶次谐波,切能量很大,
请教大家造成这种现象的原因是什么,感谢!!!
Hello,
We are working on the same product AD9746-DPG2-EBZ + AD-DAC-FMC-ADP + EVAL-SDP-CH1Z.
We suspect the same issue mentionned by zhouzhx, because we encounter the same behavior.
Could you please send us the source program or programming code of PIC18F4550…
使用AD9764 无法实现 同步,可以看看AD9746是否合适
http://www.analog.com/cn/products/digital-to-analog-converters/da-converters/ad9746.html
In a typical signal chain which you describe, in which the DAC drives a mixer (not an IQMod) the baseband I and Q channels must be modulated onto the carrier at low IF either in the DAC, or in the digital engine previous to the DAC. Since the AD9746 does…
I have a question about single-port mode of dual DAC.
Could you show me the answer of following problem.
For example AD9741,AD9743,AD9745,AD9746,AD9747,
In the case of using these dual DACs with single-port mode and only DAC1,
how should I do IQSEL pin…