Resolved. Thanks for letting us know.
Hello,
I use EVAL-AD9746 + AD-DAC-FMC-ADP + SDP-H1.
I can't generate a vector (single tone as shown as example within UG-1624), because of the error message: "No data clock was detected"
On EVAL-AD9746, the PLL of AD9516, seems to be unlocked…
Hello,
My customer wants to know if the AD9746's two DACs can be used independently.
When transmitting two real data, is it possible to transmit them independently to each DAC ?
Thanks a lot.
Hi -
The output of AD9746 and AD9783 is a current proportional to the input digital signal and the voltage reference, The evaluation board has 49.9 ohm load resistors that convert this differential current to a differential voltage. The load resistors…
Hello,
My customer use AD9746 at their system and they should use LVPECL or LVDS CLK for this DAC.
And they will use LVPECL clk source.
Below are the voltage swing spec. of AD9746 clock input & clock sources.
1. LVPECL: 0 to 2 V (1.8VL - 2.2.VH…
Hi
I have a couple of questions about AD9746.
Datasheet says that SFDR is 82, 70 and 66 dBc in the individual conditions.
Do these values represent the specifications to 2nd/3rd harmonic distortion or not ?
I wonder if these values represent the specifications…
Dear Experts,
My customer has just started evaluation of AD9746 EVM board with DPG2 board and found the following issue with DPGDownloader PC tool. Could you please help my customer to fix the following issue?
1. Evaluation system:
1) AD9746 EVM board…