FAQ
Hi all
I look to buy a DAC with at least 200MHz output frequency
So I have a question about the Eval AD9744, when I checked the datasheet in tab.2 I am not sure that I achieve 200MHz as output frequency
DAC clk is F(clock) ?? and F(out) is the output frequency…
Hello,
The Data sheet of AD9744 clock input section :“ In the differential input mode, the clock input functions as a
high impedance differential pair. The common-mode level of the CLK+ and CLK- inputs can vary from 0.75 V to 2.25 V, and
the differential…
Hi all.
I have some questions about AD9744.
1. Table 2 in the AD9744 datasheet, is the test condition AMPLITUDE 0dBFS?
2. Whether these indicators in Table 2 can be satisfied for both LFCSP packaging and TSSOP, especially when the sampling rate is 21…
landsman, can you answer this question on the AD9744 spec tables?
Assumed answered offline. Please let us know if there are further questions.
Hello Biao.H,
I am using the xilinx board KCU105 to generate the Baseband signal ,and need a DAC to converter the Baseband I/Q data ,then the Analog signal is send to the IQ modulator。
And I am looking some DACs(such as AD9122 、AD9142A),and have some question…