• AD974: Antialiasing filter

    Hi, Do I have to use for the AD974 an antialiasing filter (which
    limits the bandwitdth of the analog input signal to half of the
    sampling frequency) or the switched capacitor ADC doesn't need
    something like that because of its design technology…

  • My question is the same, but for two different devices, AD974 and AD7656.

    My question is the same, but for two different devices, AD974 and AD7656. I
    want an input range of at least +/-5V, and from what I understand from the
    datasheets, I can use both of the devices as single ended, i.e. I can use the
    four inputs on…

  • RE: AD974  Accuracy

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: 关于ADC和DAC隔离问题 AD974 AD5764R

    This question has been closed by the EZ team and is assumed answered.
  • RE: AD974 giving only 8bit data

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: how to interface AD974 with 8-bit avr microcontroller

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • EVAL-AD974CB

    Hi,

    We are using a legacy design with AD974 ADC. We wanted to modify the design and were wondering if EVAL-AD974CB is still available? Or can we get PCB design files for EVAL-AD974CB.

    Thank you.

  • AD5764_SYNC pin as CS.

    Here I have a application which used AD974 and AD5764, and I want to use MCU's
    one SPI Port to control the two chips. That requires the two chips to have Chip
    Select, then I can control the two chips separately. AD974 has CS Pin. But for

  • About AD9747

    When we use the AD974, we find the data input to P2D port have 9-10 period delay with the data input to IOUT2P and IOUT2N. We want to know the reason why it happend. In the figure,  Channel 1(yellow) is the data input curve, Channel 2(red) is the Voltage…