• RE: Connecting DAC Evaluation Boards to Xilinx Development Boards

    HI Jigg1777,

    The documentation for the AD9739A and Xilinx platform is available on our wiki at: http://wiki.analog.com/resources/fpga/xilinx/interposer/ad9739a

  • AD9739A

    Can anybody help me by giving information about how generate arbitrary waveform using AD9739A?

  • RE: AD9739A-FMC-EBZ  compatibility

    I don't understand, on the wiki AD9739A Native FMC Card / Xilinx Reference Designs [Analog Devices Wiki], it is written that the AD9739A FMC support ML605, KC705, VC707, AC701 carrier and you say that Currently the only carrier supported with the…

  • RE: AD9739A-FMC-EBZ Rev C Documentation

    The documentation for the FMC card can be found here: http://wiki.analog.com/resources/fpga/xilinx/fmc/ad9739a

    More info about AD9739A eval boards can be found here: http://wiki.analog.com/resources/eval/dpg/eval-ad9739a

    Regards,

    Andrei

  • RE: ADI Reference Design for ZC702, AD9467_FMC and AD9739a

    Hallo,

    for my situation I need a custom devicetree because the zc702 is using ad9467 via fmc1 and ad9739a via fmc2. Or what did you mean with download dts?

    So I will summerize what's done by now with the basis zynq-zc702-adv7511 devicetree:

    1)…

  • AD9739A-FMC-EBZ USB SPI not working

    The PIC18F24J50-I/ML on AD9739A-FMC-EBZ(rev C) seems not working well.

    I have connected a USB cable to the AD9739A-FMC-EBZ but the AD9739A_SPI.exe (downloaded from High-Speed DAC Software Suite) couldn't recognize the device.

    Actually, the LED XCR1 isn…

  • Trouble with AD9739A-FMC-EBZ

    I got a AD9739A-FMC-EBZ from digi-key.

    when I unpack it,I found it cannot be powered up for the  two un-mounted jumper JP1/2.

    It seems like thisI have an AD9739A-FMC-EBZ and jumpers JP1 and JP2 are not installed.  Why is that?  Thank you. 

    Then I shorted…

  • SPI configuration of ADF4350

    Hi, I met a problem when I using the adf4350 on ad9739a evaluation board.

    I've tried to write the verilog code about spi configuration of the ad9739a evaluation board which has two spi devices (adf4350 and ad9739a). I'm sure that the spi code is working…

  • AD9739A Clocking

    I made PLL Module using ADF4350 and DAC Module using ADCLK914 and AD9739A.

    Because PLL Module and DAC Module is so far way, I use ADCLK914 for clock restoration.

    DAC Module is work. It is good.

    Now, I will revision DAC Module to include ADF4350.